Edit on GitHub

[ROS] Operation

GUI Program

NOTE:

  • The test is done on ROS Kinetic Kame installed in Ubuntu 16.04.
  • The test is done on ROS Melodic Moreniainstalled in Ubuntu 18.04.
  • Make sure ROS dependencies are installed before performing these instructions - Install ROS Packages
  • Make sure to run the OpenMANIPULATOR-PRO controller instructions before running the instruction below.

You can use the GUI program to manipulate OpenMANIPULATOR-PRO. Launch open_manipulator_pro_control_gui node. This program shows the status of and allows users to control OpenMANIPULATOR-PRO.

$ roslaunch open_manipulator_pro_control_gui open_manipulator_pro_control_gui.launch

To controll OpenMANIPULATOR-PRO, first click the Timer Start button.

Check the status of the OpenMANIPULATOR-PRO (joint states, kinematics pose).

To manipulate the OpenMANIPULATOR-PRO in the joint space. Enter the joint angles and total time of the trajectory. Then click the send button.

To manipulate the OpenMANIPULATOR-PRO in the task space. Enter the kinematics pose of the OpenMANIPULATOR-PRO end-effector(tool) in the task space and the total time of the trajectory. Then click the send button.

To create a drawing trajectory with OpenMANIPULATOR-PRO. First, choose the drawing trajectory type(line, circle, rhombus, heart). And enter the parameters according to the drawing trajectory type and the total time of the drawing trajectory. Then click the send button.

Teleoperation

NOTE:

  • The test is done on ROS Kinetic Kame installed in Ubuntu 16.04.
  • The test is done on ROS Melodic Moreniainstalled in Ubuntu 18.04.
  • Make sure ROS dependencies are installed before performing these instructions - Install ROS Packages
  • Make sure to run OpenMANIPULATOR-PRO controller instructions before running the instructions below.

Keyboard

TIP: Terminal can be found with the Ubuntu search icon on the top left corner of the screen. Shortcut key for Terminal is Ctrl+Alt+t.

Launch open_manipulator_pro_teleop_keyboard node for simple teleoperation test using the keyboard.

$ roslaunch open_manipulator_pro_teleop open_manipulator_pro_teleop_keyboard.launch

If the node is successfully launched, the following instruction will appear in the terminal window.

---------------------------------
Control Your OpenManipulator-PRO!
---------------------------------
w : increase x axis in task space
s : decrease x axis in task space
a : increase y axis in task space
d : decrease y axis in task space
z : increase z axis in task space
x : decrease z axis in task space

r : increase joint 1 angle
f : decrease joint 1 angle
t : increase joint 2 angle
g : decrease joint 2 angle
y : increase joint 3 angle
h : decrease joint 3 angle
u : increase joint 4 angle
j : decrease joint 4 angle
i : increase joint 5 angle
k : decrease joint 5 angle
o : increase joint 6 angle
l : decrease joint 6 angle
v : gripper open
b : gripper close
       
1 : init pose
2 : home pose
       
q to quit
-------------------------------------------------------------------------------
Present Joint Angle J1: 0.000 J2: 0.000 J3: 0.000 J4: 0.000 J5: 0.000 J6: 0.000
Present Kinematics Position X: 0.000 Y: 0.000 Z: 0.000
-------------------------------------------------------------------------------

PS4 Joystick

Install packages for teleoperation using PS4 joystick.

$ sudo apt-get install ros-kinetic-joy ros-kinetic-joystick-drivers ros-kinetic-teleop-twist-joy
$ sudo pip install ds4drv

Connect PS4 joystick to the PC via Bluetooth using the following command

$ sudo ds4drv

Enter pairing mode with PS4 by pressing and holding Playstation button + share button for 10 sec. If the light on PS4 turns blue, enter the following commands in terminal and control OpenMANIPULATOR-PRO.

$ export ROS_NAMESPACE=/open_manipulator_pro
$ roslaunch teleop_twist_joy teleop.launch
$ roslaunch open_manipulator_pro_teleop open_manipulator_pro_teleop_joystick.launch

XBOX 360 Joystick

Install packages for teleoperation using XBOX 360 joystick.

$ sudo apt-get install xboxdrv ros-kinetic-joy ros-kinetic-joystick-drivers ros-kinetic-teleop-twist-joy

Connect XBOX 360 joystick to the PC with Wireless Adapter or USB cable, and launch teleoperation packages for XBOX 360 joystick.

$ sudo xboxdrv --silent
$ export ROS_NAMESPACE=/open_manipulator_pro
$ roslaunch teleop_twist_joy teleop.launch
$ roslaunch open_manipulator_pro_teleop open_manipulator_pro_teleop_joystick.launch

MoveIt!

TIP: Terminal application can be found with the Ubuntu search icon on the top left corner of the screen. Shortcut key for terminal is Ctrl+Alt+t.

Before you launch controller using MoveIt!, check open_manipulator_pro_controller launch file in open_manipulator_pro_controller package.

  <launch>
    <arg name="use_robot_name"         default="open_manipulator_pro"/>

    <arg name="dynamixel_usb_port"     default="/dev/ttyUSB0"/>
    <arg name="dynamixel_baud_rate"    default="1000000"/>

    <arg name="control_period"         default="0.010"/>

    <arg name="use_platform"           default="true"/>

    <arg name="use_moveit"             default="false"/>
    <arg name="planning_group_name"    default="arm"/>
    <arg name="moveit_sample_duration" default="0.050"/>

    <group if="$(arg use_moveit)">
      <include file="$(find open_manipulator_pro_controller)/launch/open_manipulator_pro_moveit.launch">
        <arg name="robot_name"      value="$(arg use_robot_name)"/>
        <arg name="sample_duration" value="$(arg moveit_sample_duration)"/>
      </include>
    </group>

    <node name="$(arg use_robot_name)" pkg="open_manipulator_pro_controller" type="open_manipulator_pro_controller" output="screen" args="$(arg dynamixel_usb_port) $(arg dynamixel_baud_rate)">
        <param name="using_platform"       value="$(arg use_platform)"/>
        <param name="using_moveit"         value="$(arg use_moveit)"/>
        <param name="planning_group_name"  value="$(arg planning_group_name)"/>
        <param name="control_period"       value="$(arg control_period)"/>
        <param name="moveit_sample_duration"  value="$(arg moveit_sample_duration)"/>
    </node>

  </launch>

Parameters List : The below The following parameters can be used to load move_group package.

use_moveit is a parameter to set whether to use MoveIt!
planning_group_name is a parameter to set in setup_assistant
moveit_sample_duration is a parameter to set sampling time when joint trajectory is planned from MoveIt!

After setting all the parameters, launch the open_manipulator_pro_controller.

  $ roslaunch open_manipulator_pro_controller open_manipulator_pro_controller.launch use_moveit:=true

Warning!
When launching the controller to use MoveIt!, OpenMANIPULATOR-PRO launch file must be turned off.

Service Server List : A list of MoveIt!-related service server that open_manipulator_pro_controller has.

TIP: If you would like to use inverse kinematics with position_only, check open_manipulator_pro_moveit -> config -> kinematics.yaml and set position_only_ik parameter to True.