File: thormang3_walking_module_msgs/SetJointFeedBackGain.srv
float32 updating_duration
JointFeedBackGain feedback_gain
---
int32 result
int32 NO_ERROR = 0
int32 NOT_ENABLED_WALKING_MODULE = 2
int32 PREV_REQUEST_IS_NOT_FINISHED = 32
Description
A service that can modify joint feedback gain.
float32 updating_duration
Time duration when updating joint feedback gain.
The gains are gradually updated based on configured time.
0 or negative value will update the joint feedback gain immediately.
JointFeedBackGain feedback_gain(thormang3_walking_module_msgs/JointFeedBackGain)
The joint feedback gain to be applied
int32 result
Result of the “SetJointFeedBackGain” Service
| Name | Value | Description |
|---|---|---|
| NO_ERROR | 0x00 | There is no error. |
| NOT_ENABLED_WALKING_MODULE | 0x02 | The thormang3_walking_module is not enabled. |
| PREV_REQUEST_IS_NOT_FINISHED | 0x20 | The previous request is not finished. |