File: thormang3_walking_module_msgs/StepPositionData.msg
Message Definition
int16 moving_foot
int16 LFootMove = 1 # Left foot constant
int16 RFootMove = 2 # Right foot constant
int16 NFootMove = 3 # No foot constant
### Unit [meter, rad]
float32 foot_z_swap
float32 body_z_swap
float32 torso_yaw_angle_rad
PoseXYZRPY left_foot_pose
PoseXYZRPY right_foot_pose
PoseZRPY body_pose
Description
Position related Step Data Parameters
int16 moving_foot
Flag for Moving Foot
The flag should be set to one of the following values.
- LFootMove : constant for the left foot move
- RFootMove : constant for the right foot move
- NFootMove : constant for no foot move
float32 foot_z_swap
The swept distance by the foot on the Z axis while THORMANG3 is walking. Unit in meter.

float32 body_z_swap
The swept distance by the body on the Z axis while THORMANG3 is walking. Unit in meter.

float32 torso_yaw_angle_rad
Waist target angle for upcoming step. Unit in rad (Not supported. This parameter is not used.)
PoseXYZRPY left_foot_pose(thormang3_walking_module_msgs/PoseXYZRPY)
Target pose of the left foot for upcoming step. Unit in meter, rad.
PoseXYZRPY right_foot_pose(thormang3_walking_module_msgs/PoseXYZRPY)
Target pose of the right foot for upcoming step. Unit in meter, rad.
PoseZRPY body_pose (thormang3_walking_module_msgs/PoseZRPY)
The target COB for upcoming step. Unit in meter, rad.