• File : open_manipulator_msgs/KinematicsPose.msg

  • Compact Message Definition

    geometry_msgs/Pose  pose
    float64    max_accelerations_scaling_factor
    float64    max_velocity_scaling_factor
    float64    tolerance
    
  • Description
       This topic msessage indicates the pose of the end-effector in the task space. The end-effector is included in topic name.

    • geometry_msgs/Pose pose
         The kinematics pose of the OpenMANIPULATOR end-effector in the task space.

    • float64 max_accelerations_scaling_factor
         maximum acceleration scaling factor for making joint trajectory from MoveIt!

    • float64 max_velocity_scaling_factor
         maximum velocity scaling factor for making joint trajectory from MoveIt!

    • float64 tolerance
         tolerance for reach a kinematics pose. This parameter is used in MoveIt!