Tutorials
Creating new motion module
Instructions for applying ROBOTIS Framework to the new robot.
Description: This is the tutorial for creating a new motion module inherited from the MotionModule class of robotis_frameowrk_common package.
Overview
“Motion Module” calculates target position(or target velocity or target current) of each joint. If the Motion Module is created and added to the RobotisController of the robotis_controller pacakge, RobotisController periodically calls process() function from the Motion Module and saves calculated value to the result_ of the Motion Module. Once the RobotisController completes calculation for all registered Motion Modules, it obtains result_ from the Motion Module for each joint and transfers the value to each joint.
The following is the example of creating a simple Motion Module.
Writing the Motion Module
Go to the directory to create the motion_module_tutorial package and create the package:
$ cd ~/catkin_ws/src/ROBOTIS-THORMANG-MPC
$ catkin_create_pkg motion_module_tutorial std_msgs roscpp
The Code
Write below header and cpp files in the motion_module_tutorial package.
link motion_module_tutorial/include/motion_module_tutorial/motion_module_tutorial.h
#ifndef MOTION_MODULE_TUTORIAL_MOTION_MODULE_TUTORIAL_H_
#define MOTION_MODULE_TUTORIAL_MOTION_MODULE_TUTORIAL_H_
#include <ros/ros.h>
#include <ros/callback_queue.h>
#include <std_msgs/Int16.h>
#include <boost/thread.hpp>
#include "robotis_framework_common/motion_module.h"
namespace thormang3
{
class MotionModuleTutorial
: public robotis_framework::MotionModule,
public robotis_framework::Singleton<MotionModuleTutorial>
{
private:
int control_cycle_msec_;
boost::thread queue_thread_;
/* sample subscriber & publisher*/
ros::Subscriber sub1_;
ros::Publisher pub1_;
void queueThread();
public:
MotionModuleTutorial();
virtual ~MotionModuleTutorial();
/* ROS Topic Callback Functions*/
void topicCallback(const std_msgs::Int16::ConstPtr &msg);
void initialize(const int control_cycle_msec, robotis_framework::Robot *robot);
void process(std::map<std::string, robotis_framework::Dynamixel *> dxls, std::map<std::string, double> sensors);
void stop();
bool isRunning();
};
}
#endif /* MOTION_MODULE_TUTORIAL_MOTION_MODULE_TUTORIAL_H_*/
link motion_module_tutorial/src/motion_module_tutorial/motion_module_tutorial.cpp
#include <stdio.h>
#include "motion_module_tutorial/motion_module_tutorial.h"
using namespace thormang3;
MotionModuleTutorial::MotionModuleTutorial()
: control_cycle_msec_(8)
{
enable_ = false;
module_name_ = "test_motion_module"; // set unique module name
control_mode_ = robotis_framework::PositionControl;
result_["r_sho_pitch"] = new robotis_framework::DynamixelState();
result_["r_sho_roll"] = new robotis_framework::DynamixelState();
result_["r_el"] = new robotis_framework::DynamixelState();
}
MotionModuleTutorial::~MotionModuleTutorial()
{
queue_thread_.join();
}
void MotionModuleTutorial::initialize(const int control_cycle_msec, robotis_framework::Robot *robot)
{
control_cycle_msec_ = control_cycle_msec;
queue_thread_ = boost::thread(boost::bind(&MotionModuleTutorial::queueThread, this));
}
void MotionModuleTutorial::queueThread()
{
ros::NodeHandle ros_node;
ros::CallbackQueue callback_queue;
ros_node.setCallbackQueue(&callback_queue);
/* subscriber */
sub1_ = ros_node.subscribe("/tutorial_topic", 10, &MotionModuleTutorial::topicCallback, this);
/* publisher */
pub1_ = ros_node.advertise<std_msgs::Int16>("/tutorial_publish", 1, true);
while (ros_node.ok())
{
callback_queue.callAvailable();
usleep(1000);
}
}
void MotionModuleTutorial::topicCallback(const std_msgs::Int16::ConstPtr &msg)
{
std_msgs::Int16 msg_int16;
msg_int16.data = msg->data;
pub1_.publish(msg_int16);
}
void MotionModuleTutorial::process(std::map<std::string, robotis_framework::Dynamixel *> dxls,
std::map<std::string, double> sensors)
{
if (enable_ == false)
return;
for (std::map<std::string, robotis_framework::DynamixelState *>::iterator state_iter = result_.begin(); state_iter != result_.end();
state_iter++)
{
int32_t p_pos = dxls[state_iter->first]->dxl_state_->present_position_;
int32_t g_pos = dxls[state_iter->first]->dxl_state_->goal_position_;
}
// ...
result_["r_sho_pitch"]->goal_position_ = 0;
result_["r_sho_roll"]->goal_position_ = 0;
result_["r_el"]->goal_position_ = 0;
}
void MotionModuleTutorial::stop()
{
return;
}
bool MotionModuleTutorial::isRunning()
{
return false;
}
The Code Explanation
Let’s look into the code section by section. Motion Module is based on the Singleton Pattern.
...
class MotionModuleTutorial
: public robotis_framework::MotionModule,
public robotis_framework::Singleton<MotionModuleTutorial>
{
...
As each Instance of Motion Module Class does the same work, Singleton Pattern is used to reduce the number of Instances.
The constructor initializes the unique name and the control mode of Motion Module, as well as the repository for the result of process() function.
...
MotionModuleTutorial::MotionModuleTutorial()
: control_cycle_msec_(8)
{
enable_ = false;
module_name_ = "test_motion_module"; // set unique module name
control_mode_ = robotis_framework::PositionControl;
result_["r_sho_pitch"] = new robotis_framework::DynamixelState();
result_["r_sho_roll"] = new robotis_framework::DynamixelState();
result_["r_el"] = new robotis_framework::DynamixelState();
}
...
Next, boost::thread is used for the Motion Module to subscribe control topics independant from the main thread.
...
#include <boost/thread.hpp>
...
boost::thread queue_thread_;
...
void queueThread();
...
...
void MotionModuleTutorial::initialize(const int control_cycle_msec, robotis_framework::Robot *robot)
{
control_cycle_msec_ = control_cycle_msec;
queue_thread_ = boost::thread(boost::bind(&MotionModuleTutorial::queueThread, this));
}
...
initialize() function is called only once when the Robot Manager registers Motion Module to the RobotisController.
The example of subscriber and publisher looks like below.
...
/* sample subscriber & publisher */
ros::Subscriber sub1_;
ros::Publisher pub1_;
...
...
void MotionModuleTutorial::queueThread()
{
ros::NodeHandle ros_node;
ros::CallbackQueue callback_queue;
ros_node.setCallbackQueue(&callback_queue);
/* subscriber*/
sub1_ = ros_node.subscribe("/tutorial_topic", 10, &MotionModuleTutorial::topicCallback, this);
/* publisher*/
pub1_ = ros_node.advertise<std_msgs::Int16>("/tutorial_publish", 1, true);
while (ros_node.ok())
{
callback_queue.callAvailable();
usleep(1000);
}
}
void MotionModuleTutorial::topicCallback(const std_msgs::Int16::ConstPtr &msg)
{
std_msgs::Int16 msg_int16;
msg_int16.data = msg->data;
pub1_.publish(msg_int16);
}
...
When updating configuration of Motion Module for each joint, previously configured Motion Module could be running. Therefore, the function that checks the status of Motion Module is required along with the function that stops the Motion Module.
...
void MotionModuleTutorial::stop()
{
return;
}
bool MotionModuleTutorial::isRunning()
{
return false;
}
...
Finally, below is the process() function that is periodically called by the RobotisController.
...
void MotionModuleTutorial::process(std::map<std::string, robotis_framework::Dynamixel *> dxls,
std::map<std::string, double> sensors)
{
if (enable_ == false)
return;
for (std::map<std::string, robotis_framework::DynamixelState *>::iterator state_iter = result_.begin(); state_iter != result_.end();
state_iter++)
{
int32_t p_pos = dxls[state_iter->first]->dxl_state_->present_position_;
int32_t g_pos = dxls[state_iter->first]->dxl_state_->goal_position_;
}
// ...
result_["r_sho_pitch"]->goal_position_ = 0;
result_["r_sho_roll"]->goal_position_ = 0;
result_["r_el"]->goal_position_ = 0;
}
...
After obtaining current and target values from the argument dxls, calculated values are saved to the result.
Building your package
If the package is created with the catkin_create_pkg command, package.xml and CMakeLists.txt will be automatically generated.
package.xml
The following is the cleaned up code of the package.xml file:
link motion_module_tutorial/package.xml
<?xml version="1.0"?>
<package>
<name>motion_module_tutorial</name>
<version>0.1.0</version>
<description>The motion_module_tutorial package</description>
<maintainer email="you@yourdomain.com">Your Name</maintainer>
<license>BSD</license>
<buildtool_depend>catkin</buildtool_depend>
<build_depend>roscpp</build_depend>
<build_depend>robotis_device</build_depend>
<build_depend>robotis_framework_common</build_depend>
<run_depend>roscpp</run_depend>
</package>
Please refer to the catkin/package.xml for more details about the package.xml file.
CMakeLists.txt
The following is the cleaned up code of the CMakeLists.txt file:
link motion_module_tutorial/CMakeLists.txt
cmake_minimum_required(VERSION 2.8.3)
project(motion_module_tutorial)
find_package(catkin REQUIRED COMPONENTS
roscpp
dynamixel_sdk
robotis_device
robotis_framework_common
)
catkin_package(
INCLUDE_DIRS include
LIBRARIES motion_module_tutorial
)
include_directories(
include
${catkin_INCLUDE_DIRS}
)
add_library(motion_module_tutorial
src/${PROJECT_NAME}/motion_module_tutorial.cpp
)
Please refer to the catkin_make/CMakeLists.txt for more details about the CMakeLists.txt file.
Build
Run catkin_make within the catkin workspace:
$ cd ~/catkin_ws
$ catkin_make
Add Created Motion Module to robotis_controller
Please refer to the below link for creating a new Robot Manager and addi101012ng Motion Module to the new Robot Manager.
Reference : Creating new robot manager
Creating new sensor module
Description: This is the tutorial for creating a new sensor module inherited from the SensorModule class of robotis_frameowrk_common package.
Overview
“Sensor Module” processes obtained values from the sensor module.
If the Sensor Module is created and added to the robotis_controller of the robotis_controller pacakge, robotis_controller periodically calls process() function from the Sensor Module and saves calculated value to the sensor_result_ of the robotis_controller. Once the robotis_controller completes calculation for all registered Sensor Modules, it transfers the result to the Motion Module.
The following is the example of creating a simple Sensor Module.
Writing the Sensor Module
Go to the directory to create the sensor_module_tutorial package and create the package:
$ cd ~/catkin_ws/src/ROBOTIS-THORMANG-MPC
$ catkin_create_pkg sensor_module_tutorial std_msgs roscpp
The Code
Write below header and cpp files in the sensor_module_tutorial package.
link sensor_module_tutorial/include/sensor_module_tutorial/sensor_module_tutorial.h
#ifndef SENSOR_MODULE_TUTORIAL_SENSOR_MODULE_TUTORIAL_H_
#define SENSOR_MODULE_TUTORIAL_SENSOR_MODULE_TUTORIAL_H_
#include <ros/ros.h>
#include <ros/callback_queue.h>
#include <std_msgs/Int16.h>
#include <boost/thread.hpp>
#include "robotis_framework_common/sensor_module.h"
namespace ROBOTIS
{
class SensorModuleTutorial
: public robotis_framework::SensorModule,
public robotis_framework::Singleton<SensorModuleTutorial>
{
private:
int control_cycle_msec_;
boost::thread queue_thread_;
/* sample subscriber & publisher*/
ros::Subscriber sub1_;
ros::Publisher pub1_;
void queueThread();
public:
SensorModuleTutorial();
virtual ~SensorModuleTutorial();
/* ROS Topic Callback Functions*/
void topicCallback(const std_msgs::Int16::ConstPtr &msg);
void initialize(const int control_cycle_msec, robotis_framework::Robot *robot);
void process(std::map<std::string, robotis_framework::Dynamixel *> dxls,
std::map<std::string, robotis_framework::Sensor *> sensors);
};
}
#endif /*SENSOR_MODULE_TUTORIAL_SENSOR_MODULE_TUTORIAL_H_*/
link sensor_module_tutorial/src/sensor_module_tutorial/sensor_module_tutorial.cpp
#include <stdio.h>
#include "sensor_module_tutorial/sensor_module_tutorial.h"
using namespace ROBOTIS;
SensorModuleTutorial::SensorModuleTutorial()
: control_cycle_msec_(8)
{
module_name_ = "test_sensor_module"; // set unique module name
result_["test_sensor"] = 0.0;
}
SensorModuleTutorial::~SensorModuleTutorial()
{
queue_thread_.join();
}
void SensorModuleTutorial::initialize(const int control_cycle_msec, robotis_framework::Robot *robot)
{
control_cycle_msec_ = control_cycle_msec;
queue_thread_ = boost::thread(boost::bind(&SensorModuleTutorial::queueThread, this));
}
void SensorModuleTutorial::queueThread()
{
ros::NodeHandle ros_node;
ros::CallbackQueue callback_queue;
ros_node.setCallbackQueue(&callback_queue);
/* subscriber */
sub1_ = ros_node.subscribe("/tutorial_topic", 10, &SensorModuleTutorial::topicCallback, this);
/* publisher */
pub1_ = ros_node.advertise<std_msgs::Int16>("/tutorial_publish", 1, true);
while (ros_node.ok())
{
callback_queue.callAvailable();
usleep(1000);
}
}
void SensorModuleTutorial::topicCallback(const std_msgs::Int16::ConstPtr &msg)
{
std_msgs::Int16 msg_int16;
msg_int16.data = msg->data;
pub1_.publish(msg_int16);
}
void SensorModuleTutorial::process(std::map<std::string, robotis_framework::Dynamixel *> dxls,
std::map<std::string, robotis_framework::Sensor *> sensors)
{
uint16_t ext_port_data_1 = dxls["r_leg_an_p"]->dxl_state_->bulk_read_table_["external_port_data_1"];
uint16_t ext_port_data_2 = dxls["r_leg_an_p"]->dxl_state_->bulk_read_table_["external_port_data_2"];
// ...
result_["test_sensor"] = 0.0;
}
The Code Explanation
Let’s look into the code section by section. Sensor Module is based on the Singleton Pattern.
...
class SensorModuleTutorial
: public robotis_framework::SensorModule,
public robotis_framework::Singleton<SensorModuleTutorial>
{
...
As each Instance of Sensor Module Class does the same work, Singleton Pattern is used to reduce the number of Instances.
The constructor initializes the unique name and the control mode of Sensor Module, as well as the repository for the result of process() function.
...
SensorModuleTutorial::SensorModuleTutorial()
: control_cycle_msec_(8)
{
module_name_ = "test_sensor_module"; // set unique module name
result_["test_sensor"] = 0.0;
}
...
Next, boost::thread is used for the Sensor Module to subscribe control topics independant from the main thread.
...
#include <boost/thread.hpp>
...
boost::thread queue_thread_;
...
void queueThread();
...
...
void SensorModuleTutorial::initialize(const int control_cycle_msec, robotis_framework::Robot *robot)
{
control_cycle_msec_ = control_cycle_msec;
queue_thread_ = boost::thread(boost::bind(&SensorModuleTutorial::queueThread, this));
}
...
initialize() function is called only once when the Robot Manager registers Sensor Module to the RobotisController.
The example of subscriber and publisher looks like below.
...
/* sample subscriber & publisher */
ros::Subscriber sub1_;
ros::Publisher pub1_;
...
...
void SensorModuleTutorial::queueThread()
{
ros::NodeHandle ros_node;
ros::CallbackQueue callback_queue;
ros_node.setCallbackQueue(&callback_queue);
/* subscriber*/
sub1_ = ros_node.subscribe("/tutorial_topic", 10, &SensorModuleTutorial::topicCallback, this);
/* publisher*/
pub1_ = ros_node.advertise<std_msgs::Int16>("/tutorial_publish", 1, true);
while (ros_node.ok())
{
callback_queue.callAvailable();
usleep(1000);
}
}
void SensorModuleTutorial::topicCallback(const std_msgs::Int16::ConstPtr &msg)
{
std_msgs::Int16 msg_int16;
msg_int16.data = msg->data;
pub1_.publish(msg_int16);
}
...
Finally, below is the process() function that is periodically called by the RobotisController.
...
void SensorModuleTutorial::process(std::map<std::string, robotis_framework::Dynamixel *> dxls,
std::map<std::string, robotis_framework::Sensor *> sensors)
{
uint16_t ext_port_data_1 = dxls["r_leg_an_p"]->dxl_state_->bulk_read_table_["external_port_data_1"];
uint16_t ext_port_data_2 = dxls["r_leg_an_p"]->dxl_state_->bulk_read_table_["external_port_data_2"];
// ...
result_["test_sensor"] = 0.0;
}
...
After Bulk Reading current and target values from the argument dxls, calculated values are saved to the result.
Building your package
If the package is created with the catkin_create_pkg command, package.xml and CMakeLists.txt will be automatically generated.
package.xml
The following is the cleaned up code of the package.xml file:
link sensor_module_tutorial/package.xml
<?xml version="1.0"?>
<package>
<name>sensor_module_tutorial</name>
<version>0.1.0</version>
<description>The sensor_module_tutorial package</description>
<maintainer email="you@yourdomain.com">Your Name</maintainer>
<license>BSD</license>
<buildtool_depend>catkin</buildtool_depend>
<build_depend>roscpp</build_depend>
<build_depend>robotis_device</build_depend>
<build_depend>robotis_framework_common</build_depend>
<run_depend>roscpp</run_depend>
</package>
Please refer to the catkin/package.xml for more details about the package.xml file.
CMakeLists.txt
The following is the cleaned up code of the CMakeLists.txt file:
link sensor_module_tutorial/CMakeLists.txt
cmake_minimum_required(VERSION 2.8.3)
project(sensor_module_tutorial)
find_package(catkin REQUIRED COMPONENTS
roscpp
dynamixel_sdk
robotis_device
robotis_framework_common
)
catkin_package(
INCLUDE_DIRS include
LIBRARIES sensor_module_tutorial
)
include_directories(
include
${catkin_INCLUDE_DIRS}
)
add_library(sensor_module_tutorial
src/${PROJECT_NAME}/sensor_module_tutorial.cpp
)
Please refer to the catkin_make/CMakeLists.txt for more details about the CMakeLists.txt file.
Build
Run catkin_make within the catkin workspace:
$ cd ~/catkin_ws
$ catkin_make
Add Created Sensor Module to robotis_controller
Please refer to the below link for creating a new Robot Manager and adding Sensor Module to the new Robot Manager.
Reference : Creating new robot manager
Creating new robot manager
Description: This tutorial explains how to create a manager node to apply ROBOTIS Framework to a new robot.
[ Table of Contents ]
- Overview
- Writing the Robot Manager Node
2.1. The Code
2.2. The Code Explained- Building the Robot Manager Node
3.1.package.xml
3.2.CMakeLists.txt
3.3. Build- Config Files
4.1. Robot Information file (.robot)
4.2. Joint initialize file (.yaml)
4.3. Offset file (.yaml)- Launch
5.1..launchfile
5.2. Run
Overview
The Robot Manager is a package to apply ROBOTIS Framework to a new robot. In this tutorial, you will be instructed to create a manager node with the robotis_controller package from the ROBOTIS Framework. In addition, configuration files that contain hardware information of the robot and setting values are necessary in order to use ROBOTIS Framework. Various types of these configuration files will be introduced and their compositions will also be explained.
Create the Robot Manager Node
Go to the directory where Robot Manager package will be created, then create a manager package:
$ cd ~/catkin_ws/src/ROBOTIS-THORMANG-MPC
$ catkin_create_pkg thormang3_manager std_msgs roscpp
The Code
Create below cpp file in the thormang3_manager package.
link thormang3_manager/src/thormang3_manager.cpp
#include "robotis_controller/robotis_controller.h"
/* Sensor Module Header */
#include "thormang3_feet_ft_module/feet_force_torque_sensor_module.h"
/* Motion Module Header */
#include "thormang3_base_module/base_module.h"
#include "thormang3_action_module/action_module.h"
#include "thormang3_head_control_module/head_control_module.h"
#include "thormang3_manipulation_module/manipulation_module.h"
#include "thormang3_walking_module/walking_module.h"
using namespace thormang3;
int main(int argc, char **argv)
{
ros::init(argc, argv, "THORMANG3_Manager");
ros::NodeHandle nh;
ROS_INFO("manager->init");
robotis_framework::RobotisController *controller = robotis_framework::RobotisController::getInstance();
/* Load ROS Parameter*/
std::string offset_file = nh.param<std::string>("offset_file_path", "");
std::string robot_file = nh.param<std::string>("robot_file_path", "");
std::string init_file = nh.param<std::string>("init_file_path", "");
/* gazebo simulation*/
controller->gazebo_mode_ = nh.param<bool>("gazebo", false);
if(controller->gazebo_mode_ == true)
{
ROS_WARN("SET TO GAZEBO MODE!");
std::string robot_name = nh.param<std::string>("gazebo_robot_name", "");
if(robot_name != "")
controller->gazebo_robot_name_ = robot_name;
}
if(robot_file == "")
{
ROS_ERROR("NO robot file path in the ROS parameters.");
return -1;
}
if(controller->initialize(robot_file, init_file) == false)
{
ROS_ERROR("ROBOTIS Controller Initialize Fail!");
return -1;
}
if(offset_file != "")
controller->loadOffset(offset_file);
sleep(1);
/* Add Sensor Module*/
controller->addSensorModule((robotis_framework::SensorModule*)FeetForceTorqueSensor::getInstance());
/* Add Motion Module*/
controller->addMotionModule((robotis_framework::MotionModule*)BaseModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)ActionModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)ManipulationModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)HeadControlModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)WalkingMotionModule::getInstance());
controller->startTimer();
while(ros::ok())
{
usleep(1000*1000);
}
return 0;
}
The Code Analysis
Let’s look into the code.
#include "robotis_controller/robotis_controller.h"
/* Sensor Module Header */
#include "thormang3_feet_ft_module/feet_force_torque_sensor_module.h"
/* Motion Module Header */
#include "thormang3_base_module/base_module.h"
#include "thormang3_action_module/action_module.h"
#include "thormang3_head_control_module/head_control_module.h"
#include "thormang3_manipulation_module/manipulation_module.h"
#include "thormang3_walking_module/walking_module.h"
...
Include headers of sensor modules and motion modules that will be used in the Robot Manager.
Load ROS Parameters from configuration files.
...
/* Load ROS Parameter */
std::string offset_file = nh.param<std::string>("offset_file_path", "");
std::string robot_file = nh.param<std::string>("robot_file_path", "");
std::string init_file = nh.param<std::string>("init_file_path", "");...
If “gazebo” is set to true in the ROS Parameters, set the controller to gazebo mode.
...
/* gazebo simulation */
controller->gazebo_mode_ = nh.param<bool>("gazebo", false);
if(controller->gazebo_mode_ == true)
{
ROS_WARN("SET TO GAZEBO MODE!");
std::string robot_name = nh.param<std::string>("gazebo_robot_name", "");
if(robot_name != "")
controller->gazebo_robot_name_ = robot_name;
}
...
If the essential robot information file is missing from the ROS Parameters, the program will be terminated. RobotisController is initialized with the information from the ROS Parameters.
...
if(robot_file == "")
{
ROS_ERROR("NO robot file path in the ROS parameters.");
return -1;
}
if(controller->initialize(robot_file, init_file) == false)
{
ROS_ERROR("ROBOTIS Controller Initialize Fail!");
return -1;
}
if(offset_file != "")
controller->loadOffset(offset_file);
...
Add sensor modules and motion modules to RobotisController.
...
/* Add Sensor Module */
controller->addSensorModule((robotis_framework::SensorModule*)FeetForceTorqueSensor::getInstance());
/* Add Motion Module */
controller->addMotionModule((robotis_framework::MotionModule*)BaseModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)ActionModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)ManipulationModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)HeadControlModule::getInstance());
controller->addMotionModule((robotis_framework::MotionModule*)WalkingMotionModule::getInstance());
...
Start the Timer of RobotisController to call Process() function periodically while program is running.
...
controller->startTimer();
while(ros::ok())
{
usleep(1000*1000);
}
...
Building the Robot Manager Node
If a package is created with the catkin_create_pkg command, package.xml and CMakeLists.txt files are automatically generated.
package.xml
Below is the contents of automatically generated package.xml file with removed comments.
<?xml version="1.0"?>
<package>
<name>thormang3_manager</name>
<version>0.1.0</version>
<description>The thormang3_manager package</description>
<maintainer email="zerom@robotis.com">ROBOTIS</maintainer>
<license>GPLv2</license>
<buildtool_depend>catkin</buildtool_depend>
<build_depend>roscpp</build_depend>
<build_depend>dynamixel_sdk</build_depend>
<build_depend>robotis_framework_common</build_depend>
<build_depend>robotis_device</build_depend>
<build_depend>robotis_controller</build_depend>
<build_depend>robotis_controller_msgs</build_depend>
<build_depend>cmake_modules</build_depend>
<build_depend>thormang3_feet_ft_module</build_depend>
<build_depend>thormang3_head_control_module</build_depend>
<build_depend>thormang3_manipulation_module</build_depend>
<build_depend>thormang3_walking_module</build_depend>
<build_depend>thormang3_base_module</build_depend>
<build_depend>thormang3_action_module</build_depend>
<run_depend>roscpp</run_depend>
<run_depend>robotis_controller</run_depend>
</package>
For more details about the package.xml file, please refer to catkin/package.xml.
CMakeLists.txt
Below is the contents of automatically generated CMakeLists.txt file with removed comments and examples.
cmake_minimum_required(VERSION 2.8.3)
project(thormang3_manager)
find_package(catkin REQUIRED COMPONENTS
roscpp
dynamixel_sdk
robotis_framework_common
robotis_device
robotis_controller
robotis_controller_msgs
robotis_math
cmake_modules
ati_ft_sensor
thormang3_kinematics_dynamics
thormang3_feet_ft_module
thormang3_head_control_module
thormang3_manipulation_module
thormang3_walking_module
thormang3_base_module
)
find_package(Eigen REQUIRED)
catkin_package(
)
include_directories(
include
${Eigen_INCLUDE_DIRS}
${catkin_INCLUDE_DIRS}
)
add_executable(thormang3_manager src/thormang3_manager.cpp)
target_link_libraries(thormang3_manager
${catkin_LIBRARIES}
)
For more details about the CMakeLists.txt file, please refer to catkin_make/CMakeLists.txt.
Build
Now, run the catkin_make within the catkin_workspace
$ cd ~/catkin_ws
$ catkin_make
Config Files
Robot Information file (.robot)
The .robot file is consisted of 2 sections and it contains information of the robot.
control info
This section includes control cycle information.
- control_cycle : Control cycle in milliseconds
port info
This section includes port information that is connected with the robot.
Each line consists of three field data as shown below and they describe properties of a related port.
- PORT NAME : File name of the port
- BAUDRATE : Default baudrate for the port
- DEFAULT JOINT : The default joint to obtain information such as Control table and Protocol Version when each port performs SyncWrite/BulkRead.
device info
This section includes hardware device information of the robot.
Each line consists of seven field data as shown below and they describe properties of a related device.
- TYPE : Type of the device (dynamixel, sensor)
- PORT NAME : File name of the port connected to the device
- ID : Allocated ID to the device
- MODEL : Model name of the device
- PROTOCOL : Protocol version to control the device
- DEV NAME : Name of the device to be used for control
- BULK READ ITEMS : The item list to be read in bulk from the device (‘,’ is a field delimiter)
.robot file example
[ control info ]
control_cycle = 8 # milliseconds
[ port info ]
# PORT NAME | BAUDRATE | DEFAULT JOINT
/dev/ttyUSB0 | 2000000 | r_arm_sh_p1
/dev/ttyUSB1 | 2000000 | l_arm_sh_p1
/dev/ttyUSB2 | 2000000 | r_leg_hip_y
/dev/ttyUSB3 | 2000000 | l_leg_hip_y
[ device info ]
# TYPE | PORT NAME | ID | MODEL | PROTOCOL | DEV NAME | BULK READ ITEMS
dynamixel | /dev/ttyUSB0 | 1 | H54-100-S500-R | 2.0 | r_arm_sh_p1 | present_position, present_voltage
dynamixel | /dev/ttyUSB1 | 2 | H54-100-S500-R | 2.0 | l_arm_sh_p1 | present_position, present_voltage
dynamixel | /dev/ttyUSB0 | 3 | H54-100-S500-R | 2.0 | r_arm_sh_r | present_position, present_voltage
dynamixel | /dev/ttyUSB1 | 4 | H54-100-S500-R | 2.0 | l_arm_sh_r | present_position, present_voltage
...
Joint initialize file (.yaml)
Format
JOINT_NAME1 :
CTRL_TABLE_ITEM_NAME1 : VALUE
JOINT_NAME2 :
CTRL_TABLE_ITEM_NAME1 : VALUE
CTRL_TABLE_ITEM_NAME2 : VALUE
Joint initialize file example
r_arm_sh_p1 : # H54-100-S500-R
return_delay_time : 10 # item name : value
operating_mode : 3
shutdown : 58
homing_offset : 0
torque_limit : 310
max_position_limit : 250950
min_position_limit : -250950
goal_torque : 310
goal_velocity : 0
goal_acceleration : 0
position_p_gain : 32
velocity_p_gain : 180
velocity_i_gain : 452
l_arm_sh_p1 : # H54-100-S500-R
return_delay_time : 10
operating_mode : 3
shutdown : 58
homing_offset : 0
torque_limit : 310
max_position_limit : 250950
min_position_limit : -250950
goal_torque : 310
goal_velocity : 0
goal_acceleration : 0
position_p_gain : 32
velocity_p_gain : 180
velocity_i_gain : 452
r_arm_sh_r : # H54-100-S500-R
return_delay_time : 10
operating_mode : 3
shutdown : 58
homing_offset : 0
torque_limit : 310
max_position_limit : 250950
min_position_limit : -250950
goal_torque : 310
goal_velocity : 0
goal_acceleration : 0
position_p_gain : 32
velocity_p_gain : 180
velocity_i_gain : 452
...
Offset file (.yaml)
offset:
head_p: 0
head_y: 0
l_arm_grip: 0
l_arm_el_y: 0
l_arm_sh_p1: 0
l_arm_sh_p2: 0
l_arm_sh_r: 0
l_arm_wr_p: 0
l_arm_wr_r: 0
l_arm_wr_y: 0
l_leg_an_p: 0
l_leg_an_r: 0
l_leg_hip_p: 0
l_leg_hip_r: 0
l_leg_hip_y: 0
l_leg_kn_p: 0
r_arm_grip: 0
r_arm_el_y: 0
r_arm_sh_p1: 0
r_arm_sh_p2: 0
r_arm_sh_r: 0
r_arm_wr_p: 0
r_arm_wr_r: 0
r_arm_wr_y: 0
r_leg_an_p: 0
r_leg_an_r: 0
r_leg_hip_p: 0
r_leg_hip_r: 0
r_leg_hip_y: 0
r_leg_kn_p: 0
torso_y: 0
init_pose_for_offset_tuner:
head_p: 0
head_y: 0
l_arm_el_y: 0
l_arm_grip: 0
l_arm_sh_p1: 0
l_arm_sh_p2: 0
l_arm_sh_r: 1.570796326794897
l_arm_wr_p: 0
l_arm_wr_r: 0
l_arm_wr_y: 0
l_leg_an_p: 0
l_leg_an_r: 0
l_leg_hip_p: 0
l_leg_hip_r: 0
l_leg_hip_y: 0
l_leg_kn_p: 0
r_arm_el_y: 0
r_arm_grip: 0
r_arm_sh_p1: 0
r_arm_sh_p2: 0
r_arm_sh_r: -1.570796326794897
r_arm_wr_p: 0
r_arm_wr_r: 0
r_arm_wr_y: 0
r_leg_an_p: 0
r_leg_an_r: 0
r_leg_hip_p: 0
r_leg_hip_r: 0
r_leg_hip_y: 0
r_leg_kn_p: 0
torso_y: 0
Launch
Create the .launch file to pass the configuration file paths as parameters when running the Robot Manager.
.launch file
<?xml version="1.0" ?>
<launch>
<arg name="use_imu" default="true"/>
<arg name="use_lidar" default="true" />
<param name="gazebo" value="false" type="bool"/>
<param name="gazebo_robot_name" value="thormang3"/>
<param name="offset_file_path" value="$(find thormang3_manager)/config/offset.yaml"/>
<param name="robot_file_path" value="$(find thormang3_manager)/config/THORMANG3.robot"/>
<param name="init_file_path" value="$(find thormang3_manager)/config/dxl_init.yaml"/>
<param name="ft_data_path" value="$(find thormang3_manager)/config/ft_data.yaml"/>
<param name="ft_calibration_data_path" value="$(find thormang3_manager)/config/ft_calibration_data.yaml"/>
<!-- imu sensor package -->
<include file="$(find imu_3dm_gx4)/launch/imu.launch" if="$(arg use_imu)"/>
<!-- lidar -->
<include file="$(find thormang3_description)/launch/thor_laserscan.launch" if="$(arg use_lidar)"/>
<!-- THORMANG3 Manager -->
<node name="thormang3_manager" pkg="thormang3_manager" type="thormang3_manager" output="screen"/>
<!-- Robot Model & TF -->
<include file="$(find thormang3_description)/launch/thormang3_mpc.launch"/>
</launch>
Run
Execute the .launch file with the roslaunch command.
$ roslaunch thormang3_manager thormang3_manager.launch