Edit on GitHub

DREAM SET B

Introduction

ROBOTIS DREAM is an entry level robotics kit optimized for learning and teaching robotics.

Set B combines the parts from the existing products ROBOTIS DREAM Level 3 and Level 4, and expands on Set A to take robotics education to a higher level.

CAUTION : ROBOTIS DREAM SET B requires parts from ROBOTIS DREAM SET A. Please make sure to purchase SET A to build the robots in SET B. Users must program the robots or download the program into the controller(CM-150) to operate the robot. To download programs, you will need the USB cable included in SET A.

Part List

Examples

For more information assembly and operation, please refer to the ROBOTIS DREAM SET B workbook. The controller initially comes with the comprehensive program pre-installed in it. To create your own program or download, click here to read more on How to Download Task code. You will need the USB cable to download the programs. This is included in ROBOTIS DREAM SET A.

Robot TASK Code
1. Probing Car
Download
2. Electric Guitar
Download
3. Flag Game Robot
Download
4. War Robot
Download