Edit on GitHub

OLLO INVENTOR

Introduction

Create robots using the controller, geared motors, sensors, and servo motors and perform basic programming. Through 12-session curriculum, learn programming and experiment on wireless communication, the concept of control, sensors and various module applications.

Part List

Quick Start

ZIGBee Wireless Control

ZIGBee

Zig-100/110

ZIG-100/110 uses ZIGBee for wireless communication. ZIGBee, like Bluetooth, is the communication technology commonly used in Personal Area Network (PAN). The communication quality of ZIGBee is better than that of IR, so it allows many users to control their robots without interferences.

CAUTION : Please note that not all products include a zigbee module and may need to be purchased separately.

Controller & ZIGBee

OLLO and Bioloid both use the RC-100, which uses IR communication method. To upgrade to the Zigbee communication method, you must purchase the ZIG-110 set separately. The ZIG-110 set includes one Zig-100 module, which is attached to the RC-100, and one Zig-110 module which is attached to the Controller.

NOTE : The modules in a single Zigbee set have been preconfigured to communicate with each other. Therefore, a module from one set may not work with a module from another set. Please be careful not to mix them up.

ZIG-100 installed in RC-100 ZIG-110 installed in CM-100
Zig-100_RC-100 Zig-110_CM-100
ZIG-110 installed in CM-510 ZIG-100 installed in CM-5
Zig-110_CM-510 Zig-100_CM-5

[Download]

Please refer to Inventor Learning Material on How to Assemble or motions during the execution for each example.

Also, please refer to How to Download of task code for more information.

I-1 TASK Code Description
1. Crossing Gate
I-1-1
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
2. Bump Car
I-1-2
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
3. Probing Car
I-1-3
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
4. Guitar
I-1-4
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
I-2 TASK Code Description
5. Bird
I-2-1
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
6. Crane
I-2-2
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
7. Combat Car
I-2-3
Download
Download
Example program for assembly check
Example program for robot
8. Tank
I-2-4
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
I-3 TASK Code Description
9. Flag Game
I-3-1
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
10. Battle Bug
I-3-2
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
11. Knight
I-3-3
Download
Download
Download
Example program for assembly check
Example program for programming
Example program for robot
12. Racing Car
I-3-4
Download
Download
Download
Download
Example program for assembly check
Example program for programming 1
Example program for programming 2
Example program for robot