Edit on GitHub

High Speed Geared Motor

Introduction

It is the motor used in OLLO; it is connected to CM-100, and the direction of spin and the speed of spin can be adjusted through port control. It can be operated as general DC motors by connecting OLLO switch and the battery box.

Compatibility Guide Controller Compatibility

Specifications

Pinout

  1. MOT-
  2. MOT+

Caution Cables can may be damaged when not properly connected (i.e. wrong orientation), or use of excessive force during connection.

Tutorials

Videos