Edit on GitHub
Getting Started DYNAMIXEL Easy SDK with OpenRB-150 tutorial Kit
- In this chapter, you will use the Dynamixel Easy SDK with the OpenRB-150 Tutorial Kit to make the motor move.
Requirements
Download and Build SDK
- Download the latest version of the Dynamixel Easy SDK from the GitHub repository
git clone https://github.com/ROBOTIS-GIT/DynamixelSDK.git - Build the SDK by following the instructions below
cd DynamixelSDK/c++/build/linux64 sudo make install - Successful output log:
mkdir -p ./.objects/ g++ -shared -fPIC -m64 -o ./libdxl_x64_cpp.so ./.objects/group_bulk_read.o ./.objects/group_bulk_write.o ./.objects/group_sync_read.o ./.objects/group_sync_write.o ./.objects/group_fast_bulk_read.o ./.objects/group_fast_sync_read.o ./.objects/group_handler.o ./.objects/packet_handler.o ./.objects/port_handler.o ./.objects/protocol1_packet_handler.o ./.objects/protocol2_packet_handler.o ./.objects/port_handler_linux.o ./.objects/connector.o ./.objects/control_table.o ./.objects/motor.o ./.objects/dynamixel_error.o ./.objects/group_executor.o -lrt cp "./libdxl_x64_cpp.so" "/usr/local/lib/libdxl_x64_cpp.so" ln -s "/usr/local/lib/libdxl_x64_cpp.so" "/usr/local/lib/libdxl_x64_cpp.so.2" ln -s "/usr/local/lib/libdxl_x64_cpp.so" "/usr/local/lib/libdxl_x64_cpp.so.2.0" ln -s "/usr/local/lib/libdxl_x64_cpp.so" "/usr/local/lib/libdxl_x64_cpp.so.2.0.0" cp -r ../../include/dynamixel_sdk/* /usr/local/include/dynamixel_sdk cp -r ../../include/dynamixel_easy_sdk/* /usr/local/include/dynamixel_easy_sdk cp -r ../../../control_table /usr/local/share/dynamixel_sdk/ ldconfig
Hardware Setup
- Connect the OpenRB-150 to the Dynamixel using a TTL cable, and connect it to your computer using a USB-C cable.

Move Motor to target position
- Create a new C++ source file named
move_motor.cppand open it in your favorite code editor.touch move_motor.cpp - Copy and paste the following code into the
move_motor.cppfile.#include "dynamixel_easy_sdk/dynamixel_easy_sdk.hpp" int main(){ dynamixel::Connector connector("/dev/ttyACM0", 57600); std::unique_ptr<dynamixel::Motor> motor1 = connector.createMotor(1); int target_position = 2000; motor1->enableTorque(); motor1->setGoalPosition(target_position); } - Build the
move_motor.cppfile and execute the compiled binary.g++ -o move_motor move_motor.cpp -ldxl_x64_cpp ./move_motor