Advanced Tutorials
Real-Time Ball Detection with YOLOv8 and OpenVINO on ROBOTIS-OP3
This tutorial provides a comprehensive guide to implementing real-time ball detection on the ROBOTIS-OP3 humanoid robot using the YOLOv8 object detection model and Intel OpenVINO toolkit. The goal is to transition from traditional computer vision methods to a deep learning-based approach, significantly improving detection accuracy and robustness in dynamic sports environments.
Limitations and Problems of Existing Methods
The current ball detection method of ROBOTIS-OP3 relies on multi-stage manual feature extraction and rule-based processing. This approach sequentially applies HSV color space filtering, morphological operations, and Hough circle transform to detect balls. However, this approach reveals several serious limitations.
- Vulnerability of color-based filtering: Dramatic degradation in detection performance when the ball’s color changes due to lighting variations, shadows, reflections, etc.
- Lack of response to shape changes: Hough circle transform assumes perfect circular objects, so it fails to detect when balls appear elliptical due to motion blur from high-speed movement or when balls are partially occluded.
- Complexity of parameter adjustment: 23 different parameters must be manually adjusted according to the environment, which greatly limits the system’s versatility.
Deep Learning-Based Object Detection Solution
Deep learning-based object detection models provide an innovative approach that can fundamentally solve the limitations of traditional methods.
- Automatic feature learning: Deep learning models automatically learn complex features and patterns from large amounts of data instead of manually designed features. This enables robust detection performance even under various lighting conditions, viewpoint changes, and partial occlusion situations.
- Real-time processing performance: YOLO (You Only Look Once) series models perform object detection with a single network pass, enabling real-time processing and efficient operation even on high-resolution videos.
- Utilization of transfer learning: By applying transfer learning based on pre-trained models, high performance can be achieved with relatively small amounts of specialized data.
Necessity and Expected Effects of System Transition
The transition from existing rule-based systems to deep learning-based object detection represents not just a technical upgrade but a fundamental paradigm shift.
- Performance improvement: Latest deep learning models achieve high detection accuracy and show stable performance even in complex situations that are difficult to solve with traditional methods.
- Improved maintainability: System performance can be improved through data-centric approaches instead of complex parameter adjustments, and adaptation to new environments can be automated through retraining.
- Securing scalability: Once built, deep learning models can be easily applied to various environments and are easy to integrate with additional object detection tasks.
Under this background, this tutorial will provide step-by-step guidance on the specific methods and actual implementation process for transitioning from existing traditional computer vision-based ball detection systems to state-of-the-art deep learning-based object detection models.
Lightweight Object Detection Model Selection and Performance Analysis
One of the most important decisions in building a deep learning-based ball detection system is selecting an appropriate object detection model. In real-time sports environments, the balance between accuracy and speed is crucial, and hardware constraints must also be considered.
YOLO Series Model Performance Comparison
Let’s compare major candidates from the YOLO series, which is currently the most widely used real-time object detection model.
| Model | Parameters | mAP@0.5-0.95 | CPU Inference Time | GPU Inference Time |
|---|---|---|---|---|
| YOLOv5n | 2.6M | 28.0% | 73.6ms | 1.12ms |
| YOLOv8n | 3.2M | 37.3% | 80.4ms | 1.47ms |
| YOLOv8s | 11.2M | 44.9% | 128.4ms | 2.66ms |
| YOLOv8m | 25.9M | 50.2% | 234.7ms | 5.86ms |
| YOLOv8l | 43.7M | 52.9% | 375.2ms | 9.06ms |
YOLOv8 Advantage: The YOLOv8 series achieves 9-10% higher mAP compared to YOLOv5 models of the same size, with YOLOv8n showing 33% improved accuracy over YOLOv5n. This is the result of latest architectural improvements, enabling more stable detection performance in complex sports environments.
Comparison with Lightweight Models
Comparison with lightweight models for mobile and edge devices is also important:
| Model | Size | Inference Time | Average Precision |
|---|---|---|---|
| EfficientDet-Lite0 | 4.4MB | 37ms | 25.69% |
| EfficientDet-Lite4 | 19.9MB | 260ms | 41.96% |
| SSD MobileNetV2 | 6.7MB | 24ms | 20.2% |
| YOLOv8n | - | 80.4ms | 37.3% |
EfficientDet and SSD MobileNet series have smaller model sizes and faster inference speeds, but show significant differences in accuracy compared to YOLOv8. Especially considering the complex backgrounds and fast movements in sports environments, these accuracy differences greatly affect practicality.
Performance Improvement through OpenVINO Optimization
Using Intel OpenVINO toolkit can improve YOLOv8 model CPU inference speed by up to 3 times. This is key technology that enables real-time processing even in environments without GPUs.
- Optimization effect: For YOLOv8m model, OpenVINO optimization can reduce inference time from 234.7ms to about 78ms, achieving 12-13FPS performance even on a single CPU.
OpenVINO automatically utilizes various hardware including Intel CPUs, integrated GPUs, and VPUs to provide additional performance improvements. This allows maximum utilization of available hardware resources without code changes.
Final Model Selection
Based on comprehensive analysis, using YOLOv8m model with OpenVINO optimization is the optimal choice.
- Accuracy advantage: Provides the highest detection accuracy among real-time models with 50.2% mAP, ensuring stable performance in complex sports environments.
- Real-time performance: Achieves real-time processing goals even on CPU through OpenVINO optimization, enabling efficient operation without separate GPUs.
- Robustness: Maintains consistent detection performance under various lighting conditions and complex backgrounds, fundamentally solving traditional method limitations.
- Scalability: Easy customization for specific sports or environments through transfer learning based on pre-trained models.
Through this selection, we can overcome the limitations of existing HSV + Hough transform methods and build a ball detection system that simultaneously satisfies the high accuracy and real-time performance required in actual sports environments.
Environment Setup
- Python Environment: Create a Python virtual environment to prevent package conflicts.
sudo apt install python3.12-venv
python3 -m venv ~/yolo_env
source ~/yolo_env/bin/activate
pip install --upgrade pip
- Ultralytics YOLOv8 Installation:
pip install ultralytics
pip install typeguard
After installation, loading the model with YOLO('yolov8m.pt') will automatically download pre-trained weights.
- OpenVINO Installation: Use Intel’s PyPI distribution for OpenVINO acceleration. After installing OpenVINO runtime, check available devices.
pip install openvino
python3 -c "from openvino import Core; print(Core().available_devices)"
- ICD (Installable Client Driver) Installation: Driver system that enables OpenCL parallel computing on Intel integrated graphics cards
sudo apt install intel-opencl-icd
- NumPy Version Downgrade:
- Binary compatibility issues occur due to version mismatch between NumPy version installed in virtual environment (NumPy 2.2.6) and NumPy version used when building
cv_bridge, one of ROS2 Jazzy’s core libraries (typically NumPy 1.x version). - Need to downgrade NumPy version in
yolo_envvirtual environment to version below 2.0 compatible withcv_bridge
- Binary compatibility issues occur due to version mismatch between NumPy version installed in virtual environment (NumPy 2.2.6) and NumPy version used when building
- Activate
yolo_envvirtual environment (skip if already activated):
source ~/yolo_env/bin/activate
- Downgrade NumPy version:
pip install "numpy<2.0"
ROS2 Package Creation and Node Implementation (YOLOv8m + OpenVINO-based Ball detection)
This section explains the complete process of creating a ROS2 package from scratch for use in ROBOTIS-OP3, completing and running a YOLOv8m + OpenVINO-based ball detection node.
1. ROS2 Package Creation (Python-based)
cd ~/robotis_ws/src
ros2 pkg create op3_advanced_detector \
--build-type ament_python \
--dependencies rclpy std_msgs sensor_msgs geometry_msgs cv_bridge op3_ball_detector_msgs
2. Package Directory Structure
The created op3_advanced_detector directory has the following structure:
op3_advanced_detector/
├── op3_advanced_detector/
│ └── __init__.py
├── package.xml
└── setup.py
3. Node Basic File Creation
The final created op3_advanced_detector directory has the following structure:
op3_advanced_detector/
├── config/
│ ├── camera_param.yaml
│ └── detector_config.yaml
├── launch/
│ ├── advanced_detector.launch.py
│ └── ball_detector_from_usb_cam.launch.py
├── op3_advanced_detector/
│ ├── __init__.py
│ └── op3_advanced_detector.py
├── resource/
│ └── op3_advanced_detector
├── package.xml
├── setup.cfg
└── setup.py
Code Structure and Description
Main Class: OP3AdvancedDetector class
class OP3AdvancedDetector(Node):
"""Advanced object detector for ROBOTIS OP3"""
Key Features:
- Inherits ROS2 Node for integration with ROS system
- Real-time ball detection based on YOLO v8 + OpenVINO
- Built-in performance optimization and monitoring functions
Class Constants:
SUPPORTED_MODELS = {'yolov8n', 'yolov8s', 'yolov8m', 'yolov8l', 'yolov8x'}
DEFAULT_INPUT_SIZE = (320, 320)
# === Class constants ===
BALL_CLASS_ID = 32 # COCO sports ball class
DEFAULT_CONF_THRESHOLD = 0.25
DEFAULT_IOU_THRESHOLD = 0.5
MAX_DETECTIONS = 3 # Maximum number of balls to detect for better performance
Initialization Functions
__init__(self): Main Constructor
def __init__(self):
super().__init__('op3_advanced_detector')
# === Initialization sequence ===
self._init_parameters()
self._setup_environment()
self._init_ros_interfaces()
self._init_detection_model()
self._init_performance_tracking()
self.get_logger().info(f"✅ Ball Detector ready | {self.device_info}")
Role:
- ROS2 node initialization
- Execute 5-stage initialization process
- Output system ready message
Why initialization order is important:
- Parameters first: Basis for all other settings
- Environment setup: System variables for performance optimization
- ROS interfaces: Build communication channels
- AI model: Most time-consuming task
- Performance tracking: Prepare for post-execution monitoring
_init_parameters(self): ROS2 Parameter Initialization
def _init_parameters(self) -> None:
"""Initialize ROS2 parameters and configuration"""
# Declare ROS2 parameters
params = [
('yolo_model', 'yolov8s'),
('openvino_precision', 'FP32'),
('camera_topic', '/usb_cam_node/image_raw'),
('confidence_threshold', 0.25),
('iou_threshold', 0.5),
('input_size', [320, 320]),
('frame_skip', 2),
('debug_mode', True),
('enable_performance_log', True)
]
for name, default in params:
self.declare_parameter(name, default)
Key Functions:
- Parameter declaration: Register with ROS2 parameter system
- Value validation: Input value validity check
- Default value setting: Provide safe default settings
Key Parameter Description:
| Parameter | Default | Description | Impact |
|---|---|---|---|
yolo_model |
‘yolov8s’ | YOLO model to use | Accuracy vs speed |
confidence_threshold |
0.25 | Detection confidence threshold | Sensitivity control |
input_size |
Input image size | Performance vs accuracy | |
frame_skip |
2 | Processing frame interval | CPU usage |
_setup_environment(self): System Environment Optimization
def _setup_environment(self) -> None:
"""System environment optimization"""
# Multithreading optimization
env_vars = {
'OMP_NUM_THREADS': '2',
'MKL_NUM_THREADS': '2',
'NUMEXPR_NUM_THREADS': '2',
'OV_CACHE_DIR': '/tmp/ov_cache'
}
for key, value in env_vars.items():
os.environ[key] = value
Optimization Purpose:
- Memory usage limitation: Prevent memory explosion due to multithreading
- Performance stabilization: Minimize thread contention
- Cache management: Specify OpenVINO model cache location
_init_ros_interfaces(self): ROS2 Communication Interface Setup
def _init_ros_interfaces(self) -> None:
"""Initialize ROS2 communication interfaces"""
self.bridge = CvBridge()
# Detect image topic type and create appropriate subscriber
self._setup_image_subscriber()
# Publishers - compatible with original op3_ball_detector
self.circle_pub = self.create_publisher(CircleSetStamped, '/ball_detector_node/circle_set', 10)
self.status_pub = self.create_publisher(String, '/ball_detector_node/status', 10)
# Debug publishers
self.debug_pub = (
self.create_publisher(Image, '/ball_detector_node/image_out', 10)
if self.debug_mode else None
)
# Additional publishers for backward compatibility
self.ball_pub = self.create_publisher(Point, '/ball_position', 10)
Topic Structure:
- Input:
/usb_cam_node/image_raw(camera image) - Output:
/ball_detector_node/circle_set(detected ball information)/ball_position(first ball position)/ball_detector_node/status(system status)/ball_detector_node/image_out(debug image)
_init_detection_model(self): AI Model Initialization
def _init_detection_model(self) -> None:
"""Initialize ball detection model"""
self.device_info = "Unknown"
self.is_openvino = False
# Try OpenVINO
if OPENVINO_AVAILABLE and self._try_openvino_setup():
return
# PyTorch fallback
self._setup_pytorch_model()
Model Selection Priority:
- OpenVINO (Intel optimization): Best performance
- PyTorch CPU: Compatibility backup
Image Processing Functions
image_callback(self, msg): Main Image Processing Loop
def image_callback(self, msg: Image) -> None:
"""Main image processing loop"""
self.frame_count += 1
# Frame skipping (performance optimization)
if self.frame_count % self.frame_skip != 0:
return
start_time = time.time()
try:
# Image preprocessing
cv_image = self.bridge.imgmsg_to_cv2(msg, "bgr8")
processed_img, transform_info = self._preprocess_image(cv_image)
# Store original frame for debug visualization
self._current_frame = processed_img.copy()
# Ball detection
detections = self._detect_balls(processed_img)
# Publish results
self._publish_results(detections, transform_info, cv_image.shape)
# Performance tracking
self._update_performance(time.time() - start_time, len(detections))
except Exception as e:
self.get_logger().error(f"❌ Image processing failed: {e}")
Processing Pipeline:
ROS Image → OpenCV Conversion → Preprocessing → AI Inference → Post-processing → ROS Publishing
Frame Skipping Effects:
frame_skip=2: 30fps → 15fps (50% CPU usage reduction)frame_skip=3: 30fps → 10fps (67% CPU usage reduction)
_preprocess_image(self, image): Image Preprocessing
def _preprocess_image(self, image: np.ndarray) -> Tuple[np.ndarray, Dict]:
"""Image preprocessing and return transformation info"""
h, w = image.shape[:2]
target_w, target_h = self.input_size
# Resize maintaining aspect ratio
scale = min(target_w / w, target_h / h)
new_w, new_h = int(w * scale), int(h * scale)
resized = cv2.resize(image, (new_w, new_h))
# Center padding
pad_w = (target_w - new_w) // 2
pad_h = (target_h - new_h) // 2
padded = cv2.copyMakeBorder(
resized, pad_h, target_h - new_h - pad_h,
pad_w, target_w - new_w - pad_w,
cv2.BORDER_CONSTANT, value=(114, 114, 114)
)
transform_info = {
'scale': scale,
'pad_w': pad_w,
'pad_h': pad_h,
'original_size': (w, h)
}
return padded, transform_info
Why Preprocessing is Needed:
- YOLO requirements: Square input needed
- Aspect ratio preservation: Prevent image distortion
- Standardization: Support various resolutions
Transformation Process Visualization:
Original (1280x720) → Resize (320x180) → Padding (320x320)
[ Image ] [ Image ] [ Padding ]
[ Image ]
[ Padding ]
compressed_image_callback(self, msg): Compressed Image Processing
def compressed_image_callback(self, msg: CompressedImage) -> None:
"""Compressed image processing callback"""
# ... Frame skipping ...
try:
# Decompress image
np_arr = np.frombuffer(msg.data, np.uint8)
cv_image = cv2.imdecode(np_arr, cv2.IMREAD_COLOR)
if cv_image is None:
self.get_logger().error("❌ Failed to decode compressed image")
return
# Process image using existing pipeline
processed_img, transform_info = self._preprocess_image(cv_image)
# ...
Reasons for Compressed Image Support:
- Bandwidth saving: Network transmission optimization
- Compatibility: Support various camera types
AI Model Inference Functions
_detect_balls(self, image): Execute Ball Detection
def _detect_balls(self, image: np.ndarray) -> List[Dict]:
"""Execute ball detection"""
try:
if self.is_openvino:
return self._openvino_inference(image)
else:
return self._pytorch_inference(image)
except Exception as e:
self.get_logger().error(f"❌ Detection failed: {e}")
return []
Dual Backup System:
- Primary: OpenVINO (Intel optimization)
- Secondary: PyTorch (general compatibility)
_openvino_inference(self, image): OpenVINO Inference
def _openvino_inference(self, image: np.ndarray) -> List[Dict]:
"""OpenVINO inference"""
# Input format conversion: HWC → CHW, BGR → RGB, normalize
input_tensor = cv2.cvtColor(image, cv2.COLOR_BGR2RGB)
input_tensor = input_tensor.transpose(2, 0, 1).astype(np.float32) / 255.0
input_tensor = np.expand_dims(input_tensor, 0)
# Execute inference
infer_request = self.compiled_model.create_infer_request()
infer_request.infer([input_tensor])
output = infer_request.get_output_tensor(0).data
# Post-processing
return self._postprocess_detections(output, image.shape)
OpenVINO Optimization Effects:
- Speed: 2-3x faster than PyTorch
- Memory: Efficient memory usage
- Hardware: Intel GPU/CPU dedicated optimization
Input Transformation Process:
# Original: (320, 320, 3) BGR uint8
# ↓ Color conversion
# (320, 320, 3) RGB uint8
# ↓ Axis transformation and normalization
# (3, 320, 320) RGB float32 [0-1]
# ↓ Add batch dimension
# (1, 3, 320, 320) RGB float32 [0-1]
_pytorch_inference(self, image): PyTorch Inference (Backup)
def _pytorch_inference(self, image: np.ndarray) -> List[Dict]:
"""PyTorch YOLO inference (fallback)"""
results = self.yolo_model.predict(
image,
classes=[self.BALL_CLASS_ID],
conf=self.DEFAULT_CONF_THRESHOLD,
iou=self.DEFAULT_IOU_THRESHOLD,
verbose=False,
save=False,
device='cpu'
)
detections = []
for result in results:
if result.boxes is not None:
for box in result.boxes:
x1, y1, x2, y2 = box.xyxy[0].cpu().numpy()
conf = float(box.conf[^0].cpu().numpy())
detections.append({
'bbox': (int(x1), int(y1), int(x2), int(y2)),
'confidence': conf,
'center': (int((x1 + x2) / 2), int((y1 + y2) / 2))
})
# Sort by confidence
return sorted(detections, key=lambda x: x['confidence'], reverse=True)
PyTorch Mode Features:
- Simplicity: Use high-level API
- Stability: More error handling
- Compatibility: Support various hardware
_postprocess_detections(self, output, img_shape): Detection Result Post-processing
def _postprocess_detections(self, output: np.ndarray, img_shape: Tuple) -> List[Dict]:
"""OpenVINO output post-processing"""
detections = []
# YOLOv8 output format: (1, 84, 8400)
predictions = output[^0].T # (8400, 84)
# Confidence filtering
ball_scores = predictions[:, 4 + self.BALL_CLASS_ID]
valid_mask = ball_scores > self.DEFAULT_CONF_THRESHOLD
if not np.any(valid_mask):
return detections
valid_preds = predictions[valid_mask]
valid_scores = ball_scores[valid_mask]
# Bounding box conversion (center coordinates → corner coordinates)
boxes = valid_preds[:, :4]
x_centers, y_centers = boxes[:, 0], boxes[:, 1]
widths, heights = boxes[:, 2], boxes[:, 3]
x1s = x_centers - widths / 2
y1s = y_centers - heights / 2
x2s = x_centers + widths / 2
y2s = y_centers + heights / 2
# Apply NMS
indices = cv2.dnn.NMSBoxes(
boxes.tolist(), valid_scores.tolist(),
self.DEFAULT_CONF_THRESHOLD, self.DEFAULT_IOU_THRESHOLD
)
if len(indices) > 0:
for i in indices.flatten():
x1, y1, x2, y2 = x1s[i], y1s[i], x2s[i], y2s[i]
conf = valid_scores[i]
# Minimum size filter
if (x2 - x1) > 8 and (y2 - y1) > 8:
detections.append({
'bbox': (int(x1), int(y1), int(x2), int(y2)),
'confidence': float(conf),
'center': (int((x1 + x2) / 2), int((y1 + y2) / 2))
})
# Limit to MAX_DETECTIONS
return sorted(detections, key=lambda x: x['confidence'], reverse=True)[:self.MAX_DETECTIONS]
YOLOv8 Output Structure:
Output tensor: (1, 84, 8400)
├── 1: Batch size
├── 84: [x, y, w, h] + 80 class scores
└── 8400: Number of prediction boxes (various grid sizes)
Class score positions:
- 0-3: Bounding box coordinates (x, y, w, h)
- 4-83: 80 COCO class scores
- Index 36 (4+32): Sports ball class
NMS (Non-Maximum Suppression):
- Purpose: Remove duplicate detections
- Method: Remove boxes with lower confidence among those with IoU > threshold
- Effect: Leave only one box per ball
Result Publishing Functions
_publish_results(self, detections, transform_info, original_shape): Integrated Result Publishing
def _publish_results(self, detections: List[Dict], transform_info: Dict, original_shape: Tuple) -> None:
"""Publish detection results"""
try:
# Publish CircleSetStamped message (main output)
self._publish_circle_set(detections, transform_info, original_shape)
if detections:
# Publish first ball position for backward compatibility
self._publish_ball_position(detections[^0], transform_info, original_shape)
self._publish_status(f"DETECTED:conf={detections[^0]['confidence']:.3f}")
self.ball_lost_count = 0
else:
self._handle_no_detection()
# Debug image (optional)
if self.debug_pub and self.debug_pub.get_subscription_count() > 0:
self._publish_debug_image(detections, transform_info)
except Exception as e:
self.get_logger().error(f"❌ Result publishing failed: {e}")
Publishing Priority:
- Essential: CircleSetStamped (main output)
- Compatibility: Point message (for existing systems)
- Status: System status string
- Optional: Debug image (only when subscribers exist)
_publish_circle_set(self, detections, transform_info, original_shape): Circle Information Publishing
def _publish_circle_set(self, detections: List[Dict], transform_info: Dict, original_shape: Tuple) -> None:
"""Publish CircleSetStamped message compatible with original op3_ball_detector"""
circle_msg = CircleSetStamped()
circle_msg.header.stamp = self.get_clock().now().to_msg()
circle_msg.header.frame_id = "camera_frame"
circles = []
for detection in detections:
center_x, center_y = detection['center']
bbox = detection['bbox']
# Coordinate inverse transformation: remove padding → restore scale
orig_x = int((center_x - transform_info['pad_w']) / transform_info['scale'])
orig_y = int((center_y - transform_info['pad_h']) / transform_info['scale'])
# Calculate radius from bounding box
bbox_width = bbox[^2] - bbox[^0]
bbox_height = bbox[^3] - bbox[^1]
radius = int(max(bbox_width, bbox_height) / 2 / transform_info['scale'])
# Boundary clipping
orig_w, orig_h = transform_info['original_size']
orig_x = np.clip(orig_x, 0, orig_w - 1)
orig_y = np.clip(orig_y, 0, orig_h - 1)
# NORMALIZE COORDINATES TO (-1, +1) RANGE
# top(-1), bottom(+1) for y-axis
# left(-1), right(+1) for x-axis
normalized_x = orig_x / orig_w * 2 - 1 # Convert to (-1, +1)
normalized_y = orig_y / orig_h * 2 - 1 # Convert to (-1, +1)
# Create Point message (x, y are normalized coordinates, z is radius)
point = Point()
point.x = float(normalized_x) # Normalized x (-1 ~ +1)
point.y = float(normalized_y) # Normalized y (-1 ~ +1)
point.z = float(radius) # radius in pixels
circles.append(point)
circle_msg.circles = circles
self.circle_pub.publish(circle_msg)
Coordinate Transformation Process:
1. AI output coordinates (based on 320x320)
↓
2. Remove padding: x' = x - pad_w, y' = y - pad_h
↓
3. Restore scale: x'' = x' / scale, y'' = y' / scale
↓
4. Original resolution coordinates (based on original size)
↓
5. Normalize: nx = x'' / width * 2 - 1, ny = y'' / height * 2 - 1
↓
6. Normalized coordinates (-1 ~ +1 range)
Advantages of Normalization:
- Resolution independent: Same coordinate system for any camera
- Robot control standardization: Direct connection to head movement angles
- Mathematical convenience: Simplified trigonometric calculations
_publish_ball_position(self, detection, transform_info, original_shape): Ball Position Publishing
def _publish_ball_position(self, detection: Dict, transform_info: Dict, original_shape: Tuple) -> None:
"""Publish ball position information"""
center_x, center_y = detection['center']
# Coordinate inverse transformation: remove padding → restore scale
orig_x = int((center_x - transform_info['pad_w']) / transform_info['scale'])
orig_y = int((center_y - transform_info['pad_h']) / transform_info['scale'])
# Boundary clipping
orig_w, orig_h = transform_info['original_size']
orig_x = np.clip(orig_x, 0, orig_w - 1)
orig_y = np.clip(orig_y, 0, orig_h - 1)
# NORMALIZE COORDINATES TO (-1, +1) RANGE
normalized_x = orig_x / orig_w * 2 - 1 # Convert to (-1, +1)
normalized_y = orig_y / orig_h * 2 - 1 # Convert to (-1, +1)
# Publish
point = Point()
point.x = float(normalized_x) # Normalized x (-1 ~ +1)
point.y = float(normalized_y) # Normalized y (-1 ~ +1)
point.z = detection['confidence']
self.ball_pub.publish(point)
Point Message Structure:
x: Normalized x coordinate (-1 ~ +1)y: Normalized y coordinate (-1 ~ +1)z: Detection confidence (0 ~ 1)
_publish_debug_image(self, detections, transform_info): Debug Image Publishing
def _publish_debug_image(self, detections: List[Dict], transform_info: Dict) -> None:
"""Publish debug image with detection visualizations"""
try:
# Use original frame as base for debug image
if hasattr(self, '_current_frame') and self._current_frame is not None:
# Resize debug image to match detection input size for consistency
debug_img = cv2.resize(self._current_frame, self.input_size)
else:
# Fallback: create empty image with detection input size
debug_img = np.zeros((*self.input_size[::-1], 3), dtype=np.uint8)
img_height, img_width = debug_img.shape[:2]
# Calculate appropriate text scale based on image size (smaller for 320x320)
text_scale = 0.4 # Fixed smaller scale for 320x320 resolution
text_thickness = 1
# Draw detection results directly on resized debug image (no coordinate transformation needed)
for i, detection in enumerate(detections):
# Use detection coordinates directly since debug image is same size as detection input
center_x, center_y = detection['center']
bbox = detection['bbox']
x1, y1, x2, y2 = bbox
# Ensure coordinates are within image bounds
x1 = max(0, min(x1, img_width - 1))
y1 = max(0, min(y1, img_height - 1))
x2 = max(0, min(x2, img_width - 1))
y2 = max(0, min(y2, img_height - 1))
center_x = max(0, min(center_x, img_width - 1))
center_y = max(0, min(center_y, img_height - 1))
# Color coding by detection order
color = (0, 255, 0) if i == 0 else (0, 255, 255) # Green for best, yellow for others
# Draw bounding box
cv2.rectangle(debug_img, (x1, y1), (x2, y2), color, 2)
# Draw center point
cv2.circle(debug_img, (center_x, center_y), 4, color, -1)
# Draw confidence text
conf_text = f"Ball {i+1}: {detection['confidence']:.3f}"
text_y = y1 - 10 if y1 > 20 else y2 + 20
cv2.putText(debug_img, conf_text, (x1, text_y),
cv2.FONT_HERSHEY_SIMPLEX, text_scale, color, text_thickness)
# Add performance info
fps_text = f"FPS: {self.current_fps:.1f} | Device: {self.device_info}"
cv2.putText(debug_img, fps_text, (5, 20),
cv2.FONT_HERSHEY_SIMPLEX, text_scale, (255, 255, 255), text_thickness)
# Convert and publish
debug_msg = self.bridge.cv2_to_imgmsg(debug_img, "bgr8")
debug_msg.header.stamp = self.get_clock().now().to_msg()
debug_msg.header.frame_id = "camera_frame"
self.debug_pub.publish(debug_msg)
except Exception as e:
self.get_logger().error(f"❌ Debug image publishing failed: {e}")
Debug Image Elements:
- Bounding boxes: Detected ball areas (rectangles)
- Center points: Ball center positions (circles)
- Confidence: Detection confidence (text)
- Performance info: FPS and device used (text)
- Color coding: First ball (green), others (yellow)
Performance Monitoring Functions
_update_performance(self, process_time, ball_count): Performance Update
def _update_performance(self, process_time: float, ball_count: int) -> None:
"""Update performance statistics"""
self.process_times.append(process_time)
self.fps_counter += 1
# Periodic logging (every 15 frames)
if self.fps_counter % 15 == 0:
self._log_performance(ball_count)
Performance Tracking Items:
- Processing time: Time taken to process each frame
- FPS: Frames processed per second
- Detection count: Number of balls detected per frame
_log_performance(self, ball_count): Performance Logging
def _log_performance(self, ball_count: int) -> None:
"""Log performance information"""
elapsed = time.time() - self.fps_timer
self.current_fps = 15 / elapsed
recent_times = self.process_times[-15:]
avg_ms = np.mean(recent_times) * 1000
max_ms = np.max(recent_times) * 1000
self.get_logger().info(
f"📊 {self.device_info} | FPS: {self.current_fps:.1f} | "
f"Process time: {avg_ms:.0f}ms (max: {max_ms:.0f}ms) | Balls: {ball_count}"
)
# Reset timer
self.fps_timer = time.time()
# Memory management
if len(self.process_times) > 30:
self.process_times = self.process_times[-15:]
Log Example:
📊 OpenVINO GPU | FPS: 15.1 | Process time: 62ms (max: 64ms) | Balls: 3
📊 PyTorch CPU | FPS: 12.3 | Process time: 81ms (max: 125ms) | Balls: 0
Performance Indicator Interpretation:
- FPS > 20: Real-time processing possible
- Process time < 50ms: Good performance
- Max time: Worst-case latency
Utility Functions
_try_openvino_setup(self): Attempt OpenVINO Setup
def _try_openvino_setup(self) -> bool:
"""Attempt OpenVINO model setup"""
try:
# Set model file paths
model_dir = Path(f"{self.yolo_model_name}_openvino_model")
xml_path = model_dir / f"{self.yolo_model_name}.xml"
# Create model if needed
if not xml_path.exists():
self.get_logger().info(f"⚙️ Creating OpenVINO model... ({self.yolo_model_name})")
self._create_openvino_model()
# Re-check after creation
if not xml_path.exists():
self.get_logger().warn(f"❌ OpenVINO model creation failed: {xml_path}")
return False
# Initialize OpenVINO core
self.ov_core = ov.Core()
# Select device and compile model
device = self._select_best_device()
self.ov_model = self.ov_core.read_model(str(xml_path))
self.compiled_model = self.ov_core.compile_model(self.ov_model, device)
self.device_info = f"OpenVINO {device}"
self.is_openvino = True
# Warmup
self._warmup_model()
self.get_logger().info(f"🚀 OpenVINO model loaded | Device: {device}")
return True
except Exception as e:
self.get_logger().warn(f"⚠️ OpenVINO setup failed: {e}")
return False
_create_openvino_model(self): Create OpenVINO Model
def _create_openvino_model(self) -> None:
"""Create OpenVINO optimized model"""
try:
# Load PyTorch model
yolo_model = YOLO(f"{self.yolo_model_name}.pt")
# Export to OpenVINO format
export_path = yolo_model.export(
format="openvino",
half=(self.precision == "FP16"),
imgsz=self.input_size[^0],
dynamic=False,
simplify=True
)
self.get_logger().info(f"✅ OpenVINO model created: {export_path}")
except Exception as e:
self.get_logger().error(f"❌ OpenVINO model creation failed: {e}")
raise
Model Conversion Options:
- FP16: 50% memory usage reduction, slight accuracy loss
- FP32: High accuracy, more memory usage
- Dynamic=False: Faster inference with fixed size
- Simplify=True: Remove unnecessary operations
_select_best_device(self): Select Optimal Device
def _select_best_device(self) -> str:
"""Select optimal inference device"""
try:
available_devices = self.ov_core.available_devices
# Prefer Intel GPU
if 'GPU' in available_devices:
return 'GPU'
elif 'CPU' in available_devices:
return 'CPU'
else:
return 'AUTO'
except:
return 'CPU' # Safe fallback
Device Priority:
- GPU: Intel integrated graphics (fastest)
- CPU: Intel CPU (medium performance)
- AUTO: Automatic selection (safe)
_warmup_model(self): Model Warmup
def _warmup_model(self) -> None:
"""Model warmup (remove initial latency)"""
dummy_input = np.zeros((1, 3, *self.input_size), dtype=np.float32)
try:
for _ in range(2):
infer_request = self.compiled_model.create_infer_request()
infer_request.infer([dummy_input])
self.get_logger().info("🔥 Model warmup complete")
except Exception as e:
self.get_logger().warn(f"Warmup failed: {e}")
Need for Warmup:
- Initial latency: First inference is slow due to cache loading
- Memory allocation: Pre-allocate GPU memory
- Optimization: Complete runtime optimization
Error Handling and State Management
_handle_no_detection(self): Handle Detection Failure
def _handle_no_detection(self) -> None:
"""Handle no ball detection"""
self.ball_lost_count += 1
if self.ball_lost_count > 10: # No detection for 10 consecutive frames
self._publish_status("NO_BALL")
Detection Failure Logic:
- Counter increment: Track consecutive failures
- Threshold application: 10 frames = about 0.5 seconds (30fps basis)
- Status publishing: Notify other nodes of situation
_publish_status(self, status): Status Publishing
def _publish_status(self, status: str) -> None:
"""Publish status message"""
msg = String()
msg.data = status
self.status_pub.publish(msg)
Status Message Types:
"DETECTED:conf=0.856": Detection success + confidence"NO_BALL": Detection failure (long-term)"ERROR:...": System error
Main Execution Function
main(args=None): Program Entry Point
def main(args=None):
"""Main execution function"""
rclpy.init(args=args)
try:
detector = OP3AdvancedDetector()
detector.get_logger().info("🎯 Ball Detector running... (Ctrl+C to stop)")
rclpy.spin(detector)
except KeyboardInterrupt:
print("\n👋 User terminated")
except Exception as e:
print(f"❌ System error: {e}")
finally:
try:
rclpy.shutdown()
except:
pass
Execution Flow:
- ROS initialization:
rclpy.init() - Node creation:
OP3AdvancedDetector() - Main loop:
rclpy.spin()- callback processing - Cleanup:
rclpy.shutdown()
Conclusion
In this tutorial, we solved the vulnerabilities of the HSV + Hough method with AI object detection. The YOLOv8m + OpenVINO combination enabled robust ball detection even with environmental changes and achieved real-time performance of ≥15FPS even in CPU-only environments. The code structure is easily extensible to various objects (e.g., goals, opposing players). For example, by retraining the YOLOv8 model with goal data or training additional classes, the same node can be extended to detect multiple objects.
Voice Control System Implementation
Introduction
Limitations of the Existing ROBOTIS-OP3
The ROBOTIS-OP3 is a humanoid robot with powerful hardware capabilities, but its basic software does not include the functionality to interact with the robot through voice. This meant that users could only control the robot through buttons or a remote GUI.
This tutorial provides a comprehensive guide to building a system that adds real-time Speech-to-Text and Text-to-Speech (TTS) capabilities to the ROBOTIS-OP3, allowing users to communicate with and control the robot using voice commands.
Tutorial Goals
- Implement a stable voice recognition system that works even in environments with robot motor noise.
- Build a hybrid TTS system that can handle both online and offline environments.
- Implement multi-stage filtering to prevent the echo phenomenon where TTS output is fed back into the microphone.
- Integrate the implemented voice control system with the existing OP3 demo framework.
Voice Recognition Model and TTS Selection Rationale
Voice Recognition: Vosk Engine
In this system, Vosk was chosen as the primary voice recognition engine.
| Feature | Vosk | Google Speech API | Mozilla DeepSpeech |
|---|---|---|---|
| Offline Operation | ✓ (Fully offline) | ✗ (Online required) | ✓ (Offline) |
| Model Size | 50MB (lightweight model) | N/A (Cloud) | ~200MB |
| Language Support | 20+ languages | 100+ languages | English-centric |
| Accuracy | Medium-High | Very High | Medium-High |
| Resource Usage | Low | Network dependent | Medium |
| Real-time Processing | ✓ (Streaming API) | ✓ (Streaming) | ✓ |
| Customization | ✓ (Vocabulary reconfiguration) | Limited | ✓ (Model training) |
| Ease of Installation | ✓ (pip install) | ✓ (API key required) | Complex |
| Suitability for Robot Environment | ★★★★★ | ★★☆☆☆ | ★★★☆☆ |
Reasons for choosing Vosk:
- Complete Offline Operation: All voice recognition is processed inside the NUC without an internet connection. This ensures the robot’s autonomy and fundamentally blocks issues like network latency or instability.
- Lightweight and High Performance: It uses a lightweight model of about 50MB, making it suitable for embedded systems, while enabling real-time continuous voice processing through its streaming API.
- Easy Integration: It can be easily installed with Python’s
pipand is easy to integrate into a ROS2 node.
Speech Synthesis: Multi-layered TTS System Configuration
This system adopts a hybrid approach that utilizes different TTS engines depending on the situation.
| Feature | gTTS | Festival | espeak |
|---|---|---|---|
| Offline Operation | ✗ (Online required) | ✓ (Fully offline) | ✓ (Fully offline) |
| Voice Quality | Very High (Natural speech) | Medium (Robotic) | Low (Robotic) |
| Language Support | 100+ languages | English-centric | 100+ languages |
| Ease of Installation | ✓ (pip install) | Complex (Compilation required) | ✓ (Package manager) |
| Resource Usage | Network dependent | Medium | Very Low |
| Suitability for Robot Environment | ★★★☆☆ | ★★★★☆ | ★★★★★ |
| Response Speed | Network dependent | Fast | Very Fast |
| Customization | Limited | ✓ (High) | Medium |
Role of each TTS engine:
- gTTS (Primary Engine): An online engine that uses Google’s TTS API, providing the most natural and high-quality voice. It is used preferentially in an online environment.
- Festival (1st Offline Fallback): An offline engine that automatically switches over if gTTS fails (e.g., network disconnection). It is highly stable and uses few system resources.
- espeak (2nd Offline Fallback): The final backup engine in case Festival also fails. It is very light and fast, but the voice quality is relatively robotic.
Environment Preparation and Installation
Dependency Package Installation
Open a terminal and run the following commands in order to install the necessary system libraries and Python packages.
# Update system packages
sudo apt update && sudo apt upgrade -y
# Install audio and TTS related system libraries
sudo apt install -y python3-pip portaudio19-dev python3-pyaudio
sudo apt install -y festival festival-dev espeak espeak-data
# Create and activate a Python virtual environment (recommended)
sudo apt install -y python3.12-venv
python3 -m venv ~/yolo_env
source ~/yolo_env/bin/activate
# Install Python dependencies
pip install vosk sounddevice numpy scipy librosa noisereduce
pip install gtts pygame rclpy std-msgs geometry-msgs
pip install PyYAML jinja2 setuptools typeguard
Download Vosk Model
# Create model directory
mkdir -p ~/op3_voice_tutorial/models
cd ~/op3_voice_tutorial/models
# Download and unzip the lightweight English model (approx. 45MB)
wget https://alphacephei.com/vosk/models/vosk-model-small-en-us-0.15.zip
unzip vosk-model-small-en-us-0.15.zip
mv vosk-model-small-en-us-0.15 vosk-model-small-en-us
Package Creation and Code Addition
Create ROS2 Package
# Move to workspace
cd ~/robotis_ws/src/ROBOTIS-OP3-Tutorials
# Create package
ros2 pkg create --build-type ament_python op3_voice_control \
--dependencies rclpy std_msgs geometry_msgs
Set Up Package Structure
op3_voice_control/
├── launch/
│ └── voice_control.launch.py # ROS2 launch file
├── op3_voice_control/
│ ├── __init__.py # Python package initialization
│ ├── speech_recognition_node.py # Speech recognition node
│ └── command_processor.py # Command processor node
├── scripts/
│ └── start_voice_control.sh # System start script
├── package.xml # Package metadata
└── setup.py # Python installation setup
Note: You can download the complete package source from the GitHub repository:
https://github.com/ROBOTIS-GIT/ROBOTIS-OP3-Tutorials/op3_voice_control
Modify Existing OP3 Demo Code
Some modifications to the existing demo code are required for the voice control system to interact with the OP3’s basic motion modules.
op3_demo/src/demo_node.cpp modifications:
// Add demo mode command callback for voice control
void demoModeCommandCallback(const std_msgs::msg::String::SharedPtr msg)
{
// ... existing code ...
else if(msg->data == "action")
{
desired_status = ActionDemo;
apply_desired = true;
// Enable voice control mode
action_demo->setVoiceControlMode(true);
RCLCPP_INFO(node->get_logger(), "Voice control mode enabled for action demo");
dxlTorqueChecker();
playSound(default_mp3_path + "Start motion demonstration.mp3");
if (DEBUG_PRINT)
RCLCPP_INFO(node->get_logger(), "= Start Demo Mode : %d", desired_status);
}
}
op3_demo/include/op3_demo/action_demo.h modifications:
class ActionDemo : public OPDemo
{
public:
// ... existing methods ...
void setVoiceControlMode(bool voice_mode);
// Public methods for voice control
void playAction(int motion_index);
void stopAction();
void brakeAction();
bool isActionRunning();
protected:
// ... existing members ...
bool voice_control_mode_; // Voice control mode flag
bool stop_action_executed_; // Flag to prevent duplicate stops
};
Key Code Explanation
System Architecture and Data Flow
The voice control system consists of two core nodes that communicate organically through ROS2 topics.
- Microphone Input:
sounddevicecaptures the audio stream. - speech_recognition_node:
- Applies noise filtering to the audio stream.
- Converts the filtered audio to text via the Vosk engine.
- Publishes the recognized text to the
/voice_commandtopic.
- command_processor:
- Subscribes to the
/voice_commandtopic. - Analyzes the received text to determine if it is an echo and matches it against registered command patterns.
- Publishes robot control commands to the
/robotis/action/page_numor/robotis/mode_commandtopics based on the matched command. - Simultaneously calls the TTS engine to play audio for user feedback.
- Subscribes to the
-
speech_recognition_node.py: Speech Recognition and Noise Filtering
This node is responsible for receiving microphone input in real-time and converting it to text.-
2-Stage Noise Filtering
To handle both specific frequency noises like motor sounds, a major problem in robot environments, and general background noise, a 2-stage filtering strategy is used.- Notch Filter: Precisely removes noise in specific frequency bands (50Hz, 100Hz, 200Hz, etc.) commonly generated by robot motors using
scipy.signal.iirnotch. -
Broadband Noise Reduction: Generally reduces the remaining background noise (like fan noise) not caught by the notch filter using the
noisereducelibrary.def apply_noise_filtering(self, audio_data): """Apply noise filtering""" if not self.noise_reduction: return audio_data # Type conversion audio_float = audio_data.astype(np.float32) / 32768.0 # Apply notch filter (motor noise removal) filtered_audio = audio_float for b, a in self.notch_filters: filtered_audio = signal.filtfilt(b, a, filtered_audio) # Apply advanced noise reduction try: # Use first 0.5 seconds as noise profile if len(filtered_audio) > self.sample_rate // 2: noise_sample = filtered_audio[:self.sample_rate // 2] filtered_audio = nr.reduce_noise( y=filtered_audio, sr=self.sample_rate, y_noise=noise_sample, prop_decrease=0.8 ) except Exception as e: self.get_logger().warn(f"Advanced noise reduction failed: {e}") # Convert back to int16 return (filtered_audio * 32768.0).astype(np.int16)
- Notch Filter: Precisely removes noise in specific frequency bands (50Hz, 100Hz, 200Hz, etc.) commonly generated by robot motors using
-
Asynchronous Processing: Audio Callback and Recognition Thread
audio_callback: Called automatically by thesounddevicelibrary whenever data comes in from the audio hardware. This function only applies noise filtering and puts the processed data intoself.audio_queueto prevent audio drops.recognition_loop: Runs in a separate thread and continuously checks for data accumulating in theaudio_queue. The actual recognition work of fetching data from the queue and passing it to the Vosk engine is done in this thread, so it does not interfere with real-time processing like audio capture.
-
-
command_processor.py: Command Processing and Multi-level Echo Prevention
This node acts as the brain of the system, interpreting recognized text, controlling the robot, and responding with voice.-
Multi-level Echo Cancellation Architecture
To break the feedback loop where TTS speech is fed back into the microphone, a 5-stage echo prevention system is implemented in the
voice_command_callbackfunction.- TTS Playback Status Flag (
is_speaking): Immediately ignores all incoming voice commands while TTS is active. - TTS Cooldown Timer (
tts_cooldown): Ignores commands that come in for 2.0 seconds after TTS playback finishes to prevent echoes from slight audio delays. - Echo Pattern Filtering (
is_tts_echo): If a pattern matching the system’s frequent response phrases like “entering ready mode” is detected, it is considered an echo and filtered out. - Recent TTS Text Similarity Check (
is_similar_to_recent_tts): Calculates the word similarity between recent TTS output history and the received text. If they match by 70% or more, it’s judged as an echo. - Physical Microphone Deactivation: Just before TTS playback, it publishes a “disable” message to the
/mic_controltopic, and an “enable” message after playback ends, fundamentally blocking echo influx at the hardware level. This topic is received byspeech_recognition_nodeto control the audio stream.
- TTS Playback Status Flag (
-
Flexible Command Matching
Regular expressions (
re) are used to match various forms of commands like “stand up”, “get up”, and “standup” to the same action (stand_up), enhancing user convenience. -
Duplicate Command Filtering
A cooldown of 0.5 seconds for emergency commands like
"stop"and 1.0 second for general commands is applied to prevent users from unintentionally executing the same command in quick succession. -
Non-blocking TTS Playback (
speakfunction)The process of generating and playing a TTS file can take time. If this task were handled in the main thread, the entire ROS node would freeze. To prevent this, the
speakfunction creates a separate thread calledtts_threadto handle TTS-related tasks asynchronously.def speak(self, text): """High-quality TTS speech (with echo prevention)""" def tts_thread(): with self.tts_lock: # Prevent simultaneous thread access try: self.disable_microphone() self.is_speaking = True # ... gTTS, Festival, etc. TTS playback logic ... finally: self.is_speaking = False self.enable_microphone() # Run TTS in a separate thread to avoid blocking the main node thread = threading.Thread(target=tts_thread) thread.daemon = True thread.start()
-
-
C++ Code Integration: Control Transfer through State Management
The
voice_control_mode_flag added toaction_demo.his a key state management device that prevents system malfunction by clearly distinguishing the control subject (button or voice) within the same ActionDemo mode.- When entering mode via voice:
setVoiceControlMode(true)is called fromdemo_node.cpp. This putsActionDemoin a state where it waits for an external voice command topic. - When entering mode via button:
setVoiceControlMode(false)is called from thebuttonHandlerCallbackindemo_node.cpp. In this state, the existing logic based on button input operates.
- When entering mode via voice:
-
voice_control.launch.py: Flexible System ExecutionThe launch file is designed to go beyond simply running nodes, allowing for flexible system configuration.
- Launch Arguments: Key settings like
model_pathordevice_idare exposed as launch arguments, allowing settings to be changed from the terminal, such asros2 launch … model_path:=/path/to/my/model, without modifying the code. - Virtual Environment Integration (
prefix): Theprefix='/home/robotis/yolo_env/bin/python3'setting ensures that these nodes run within the specified Python virtual environment. This is a crucial setting that prevents conflicts with system-wide installed packages and facilitates project-specific dependency management.
- Launch Arguments: Key settings like
Execution and Testing Methods
System Build and Execution
-
Build ROS2 Package
cd ~/robotis_ws colcon build --packages-select op3_voice_control -
Set Environment and Run
The provided
start_voice_control.shscript handles virtual environment activation, ROS2 environment setup, and launch file execution all at once.# Grant execution permission chmod +x ~/robotis_ws/src/ROBOTIS-OP3-Tutorials/op3_voice_control/scripts/start_voice_control.sh # Run the script ~/robotis_ws/src/ROBOTIS-OP3-Tutorials/op3_voice_control/scripts/start_voice_control.shAlternatively, you can run the launch file manually:
# Activate virtual environment source ~/yolo_env/bin/activate # Set up ROS2 environment source ~/robotis_ws/install/setup.bash # Run launch file ros2 launch op3_voice_control voice_control.launch.py
Testing
Once the system is running, you can test its functionality with the following voice commands.
- Mode Change: “action mode”, “motion mode”, “ready mode”
- Basic Actions: “stand up”, “sit down”
- Stop: “stop”, “halt”
- Emotions: “bye bye”, “clap”, “wow”
- Status Check: “status”, “how are you”
Expected Results:
- When you speak a command, the recognized text will be printed in the terminal.
- The robot will respond with voice, such as “Entering action mode”.
- The robot motion corresponding to the command will be executed.
- While the robot is speaking, it will not recognize new voice commands.
Troubleshooting Tips
-
If “Failed to initialize audio stream” error occurs:
Check if the microphone device ID is correct. You can check the list of available devices using
sounddeviceand modify thedevice_idargument in the launch file.# Check device list python3 -c "import sounddevice as sd; print(sd.query_devices())" # Run with a specific device ID (e.g., if ID is 2) ros2 launch op3_voice_control voice_control.launch.py device_id:=2 -
If voice recognition is poor:
Check if the microphone is too far away or if there is excessive ambient noise. You can test by setting the
noise_reductionparameter toFalsein thevoice_control.launch.pyfile to turn off the noise filtering feature.
Advanced Tutorials
Advanced tutorials are tested on and provided for ROBOTIS-OP3 Revision 3.
Select the 2025 ~ tab at the top of the page to view the tutorial contents.