[ROS] Simulation
NOTE:
- The test is done on
ROS Kinetic Kameinstalled inUbuntu 16.04. - The test is done on
ROS Melodic Moreniainstalled inUbuntu 18.04. - Make sure ROS dependencies are installed before performing these instructions - Install ROS Packages
Launch gazebo
Load OpenManipulator-PRO on Gazebo simulator and click on Play ▶ button.
$ roslaunch open_manipulator_p_gazebo open_manipulator_p_gazebo.launch

Enter rostopic list to list up the activated topics.
/clock
/gazebo/link_states
/gazebo/model_states
/gazebo/parameter_descriptions
/gazebo/parameter_updates
/gazebo/set_link_state
/gazebo/set_model_state
/gazebo_gui/parameter_descriptions
/gazebo_gui/parameter_updates
/open_manipulator_p/joint1_position/command
/open_manipulator_p/joint2_position/command
/open_manipulator_p/joint3_position/command
/open_manipulator_p/joint4_position/command
/open_manipulator_p/joint5_position/command
/open_manipulator_p/joint6_position/command
/open_manipulator_p/joint_states
/rosout
/rosout_agg
Controller for gazebo
Launch the open_manipulator_p_controller for gazebo simulation.
$ roslaunch open_manipulator_p_controller open_manipulator_p_controller.launch use_platform:=false
NOTE:
- To control the OpenManipulator-PRO in the Gazebo environment using the OpenManipulator-PRO Controller, the controller must set the use_platform parameter to false because it needs to send messages to gazebo instead of Platform.
- If you want to manipulate the OpenManipulator-PRO using Moveit within the Gazebo simulator, you should also convert the use_moveit to true in open_manipulator_p_controller launch file.
If the OpenManipulator-PRO controller for gazebo simulation Launched successfully, the terminal will represent below messages.
SUMMARY
========
PARAMETERS
* /open_manipulator_p/control_period: 0.01
* /open_manipulator_p/moveit_sample_duration: 0.05
* /open_manipulator_p/planning_group_name: arm
* /open_manipulator_p/using_moveit: False
* /open_manipulator_p/using_platform: False
* /rosdistro: kinetic
* /rosversion: 1.12.14
NODES
/
open_manipulator_p (open_manipulator_p_controller/open_manipulator_p_controller)
ROS_MASTER_URI=http://192.168.3.149:11311
process[open_manipulator_p-1]: started with pid [4388]
[INFO] Ready to simulate /open_manipulator_p on Gazebo
NOTE : In OpenMAIPULATOR-PRO controller for gazebo simulation, Joint and Gripper DYNAMIXEL are not enable, following messages will not be displayed :
Joint Dynamixel ID : 1, Model Name : PRO-PLUS-PH54-200-S500-R
Joint Dynamixel ID : 2, Model Name : PRO-PLUS-PH54-200-S500-R
Joint Dynamixel ID : 3, Model Name : PRO-PLUS-PH54-100-S500-R
Joint Dynamixel ID : 4, Model Name : PRO-PLUS-PH54-100-S500-R
Joint Dynamixel ID : 5, Model Name : PRO-PLUS-PH42-020-S300-R
Joint Dynamixel ID : 6, Model Name : PRO-PLUS-PH42-020-S300-R
Open an open_manipulator_p_control_gui to control OpenMANIPULATOR-P