Edit on GitHub
Task Python API
pycm Module
Here we introduce two ways to use pycm module.
import pycm # pycm should NOT be omitted in the following code
pycm.led.on(pycm.const.RED)
2.
from pycm import * # pycm should be omitted in the following code
led.on(const.RED)
We assume the SECOND case in the following description.
| Methods | Description | Parameter | Return | Example |
|---|---|---|---|---|
console(ch: int) -> None |
Configure controller’s communication channel | BLE (0) UART (1) USB (2) |
None | console(BLE) |
delay(ms: int) -> None |
Delay in milliseconds | 0 ~ 4,294,967,295 | None | delay(1000) |
millis() -> None |
Milliseconds since controller turns on | None | 0 ~ 4294967295 | pre_time = millis() |
micros() -> None |
Microseconds since controller turns on | None | 0 ~ 4294967295 | pre_time = micros() |
Submodules of pycm
| Submodules of pycm | Description |
|---|---|
| const | Constant values |
| led | LED control |
| info | Controller’s information |
| eeprom | Controller’s parameters stored in EEPROM area |
| rc | Remote control |
| etc | Miscellaneous functions |
| timer | Timer functions |
| button | Buttons |
| dxlbus | Batch controlling Dynamixel actuators |
| motion | Motion control |
| buzzer | Buzzer |
| mic | Microphone |
| imu | IMU(Inertial Measurement Unit) |
| OLLO | 5-pin port extension interface |
| DXL | Dynamixel actuator |
| rpi | Raspberry Pi interface |
Const Submodule
| Constant members of const | Description | Example |
|---|---|---|
| RED | Red color constant for controller’s RGB LED | led.on(const.RED) |
| GREEN | Green color constant for controller’s RGB LED | led.on(const.GREED) |
| BLUE | Blue color constant for controller’s RGB LED | led.on(const.BLUE) |
| ALL | White color constant for controller’s RGB LED | led.on(const.ALL) |
| OLLO_WHEEL_SPEED | Use 5-pin servo motor in wheel mode | wheel = OLLO(1, const.OLLO_WHEEL_SPEED) |
| OLLO_JOINT_POSITION | Use 5-pin servo motor in joint mode and control its position | joint = OLLO(1, const.OLLO_JOINT_POSITION) |
| OLLO_JOINT_SPEED | Use 5-pin servo motor in joint mode and control its speed | speed = OLLO(1, const.OLLO_JOINT_SPEED) |
| OLLO_IR | IR sensor 5-pin device | ir = OLLO(1, const.OLLO_IR) |
| OLLO_DMS | DMS sensor 5-pin device | dms = OLLO(1, const.OLLO_DMS) |
| OLLO_TOUCH | Touch sensor 5-pin device | touch = OLLO(1, const.OLLO_TOUCH) |
| OLLO_LED | LED module 5-pin device | led = OLLO(1, const.OLLO_LED) |
| OLLO_USER | 5-pin user device | user = OLLO(1, const.OLLO_USER) |
| OLLO_TEMPERATURE | Temperature sensor 5-pin device | temperature = OLLO(1, const.OLLO_TEMPERATURE) |
| OLLO_MAGNET | Magnet sensor 5-pin device | magnet = OLLO(1, const.OLLO_MAGNET) |
| OLLO_MOTION_DETECTION | Motion detecting sensor 5-pin device | motion_detection = OLLO(1, const.OLLO_MOTION_DETECTION) |
| OLLO_COLOR | Color sensor 5-pin device | color = OLLO(1, const.OLLO_COLOR) |
| OLLO_MOISTURE | Moisture value of Moisture-Temperature sensor 5-pin device | moisture = OLLO(1, const.OLLO_MOISTURE) |
| OLLO_MOISTURE_TEMP | Temperature value of Moisture-Temperature sensor 5-pin device | temperature = OLLO(1, const.OLLO_MOISTURE_TEMP) |
| OLLO_BRIGHTNESS | Brightness sensor 5-pin device | brightness = OLLO(1, const.OLLO_BRIGHTNESS) |
| OLLO_RED_BRIGHTNESS | Brightness of red LED of Red-Blue LED | red = OLLO(1, const.OLLO_RED_BRIGHTNESS) |
| OLLO_BLUE_BRIGHTNESS | Brightness of blue LED of Red-Blue LED | blue = OLLO(1, const.OLLO_BLUE_BRIGHTNESS) |
| V | Vertical mode | imu.imu_type(const.V) |
| H | Horizontal mode | imu.imu_type(const.H) |
| JOINT | Joint mode of Dynamixel actuator | DXL(2).mode(const.JOINT) |
| WHEEL | Wheel mode of Dynamixel actuator | DXL(3).mode(const.WHEEL) |
Led Submodule
| Methods | Description | Parameter | Return | Example |
|---|---|---|---|---|
on(color: int) -> None |
Turn on specified color of controller’s LED | color: LED name- const.RED / const.BLUE / const.GREEN |
None | led.on(const.RED) |
off(color: int) -> None |
Turn off specified color of controller’s LED | color: LED name- const.RED / const.BLUE / const.GREEN |
None | led.off(const.RED \| const.GREEN) |
set(color: int) -> None |
Set controller’s LED as specified color | color: LED name- const.RED / const.BLUE / const.GREEN |
None | led.set(const.BLUE) |
toggle(color: int) -> None |
Toggle specified color of controller’s LED | color: LED name- const.RED / const.BLUE / const.GREEN |
None | led.toggle(const.GREEN \| const.BLUE) |
Info Submodule
| Methods of info submobule | Description | Example |
|---|---|---|
model_number() -> int |
Return controller’s model number (450) | info.model_number() |
fw_version() -> int |
Return controller’s firmware version | info.fw_version() |
id() -> int |
Return controller’s id (200) | info.id() |
boot_version() -> int |
Return controller’s bootloader version | info.boot_version() |
voltage() -> int |
Return controller’s voltage (unit: 0.1V) | info.voltage() |
temperature() -> int |
Return controller’s temperature (unit: °C) | info.temperature() |
address() -> str |
Return controller’s BLE MAC address as string | info.address() |
EEPROM Submodule
| Methods of eeprom submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
dxl_baud() -> int |
Return controller’s dynamixel bus baudrate | None | 0 : 9600bps 1 : 57600bps 2 : 115200bps 3 : 1000000bps 4 : 2000000bps 5 : 3000000bps 6 : 4000000bps 7 : 4500000bps |
eeprom.dxl_baud() |
dxl_baud(baud: int) -> None |
Set controller’s dynamixel bus baudrate | 0 : 9600bps 1 : 57600bps 2 : 115200bps 3 : 1000000bps 4 : 2000000bps 5 : 3000000bps 6 : 4000000bps 7 : 4500000bps |
None | eeprom.dxl_baud(3) |
uart_baud() -> int |
Return controller’s uart port baudrate | None | 0 : 9600bps 1 : 57600bps 2 : 115200bps 3 : 1000000bps 4 : 2000000bps 5 : 3000000bps 6 : 4000000bps 7 : 4500000bps |
eeprom.uart_baud() |
uart_baud(baud: int) -> None |
Set controller’s uart port baudrate | 0 : 9600bps 1 : 57600bps 2 : 115200bps 3 : 1000000bps 4 : 2000000bps 5 : 3000000bps 6 : 4000000bps 7 : 4500000bps |
None | eeprom.uart_baud(1) |
imu_type() -> int |
Return controller’s imu direction type | None | 0 : VERTICAL 1 : HORIZONTAL |
eeprom.imu_type() |
imu_type(type:int) -> None |
Set controller’s imu direction type | const.V const.H |
None | eeprom.imu_type(const.V) |
RC Submodule
| Methods of rc submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
port(ch: int) -> None |
Set controller’s remote control channel | BLE (0) UART (1) USB (2) |
None | rc.port(BLE) |
received() -> bool |
Return if reveived a new remote control packet | None | True : new packet arrived False : new packet not arrived |
rc.received() |
read() -> int |
Return last received remote control packet value | None | 0 ~ 65535 | rc.read() |
write(data: int) -> None |
Send remote control packet value | 0 ~ 65535 | None | rc.write(128) |
Etc Submodule
| Methods of etc submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
print_screen(val: int) -> None |
Print an integer value to task monitor with a space | -2,147,483,647 ~ 2,147,483,647 | None | etc.print_screen(100) |
println_screen(val: int) -> None |
Print an integer value to task monitor with a new line | -2,147,483,647 ~ 2,147,483,647 | None | etc.println_screen(100) |
print_string(str: str) -> None |
Print a string to task monitor with a space | max 19 bytes | None | etc.print_string("Hello world!") |
println_string(str: str) -> None |
Print a string to task monitor with a new line | max 19 bytes | None | etc.println_string("Hello world!") |
port(ch: int) -> None |
Set controller’s print screen channel | BLE (0) UART (1) USB (2) |
None | etc.port(BLE) |
Timer Submodule
| Methods of etc submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
init(ms: int, func: function) -> None |
Register a callback function which will be called periodically Only one function can be registered |
msfunction calling period in millisecond funcfunction to be called |
None | timer.init(1000, func) |
start() -> None |
Start the registered function callback process | None | None | timer.start() |
stop() -> None |
stop the registered function callback process | None | None | timer.stop() |
Button Submodule
| Methods of button submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
pressed() -> bool |
Return if controller’s user button is pressed | None | True : pressed False : not pressed |
button.pressed() |
released() -> bool |
Return if controller’s user button is released after pressed | None | True : release event happened False : release event not happened |
button.released() |
millis() -> int |
Return last pressed time in milliseconds | None | 0 ~ 65535 | button.millis() |
seconds() -> int |
Return last pressed time in seconds | None | 0 ~ 255 | button.seconds() |
Dxlbus Submodule
| Methods of dxlbus submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
power_on() -> None |
Turn on power for dynamixel bus | None | None | dxlbus.power_on() |
power_off() -> None |
Turn off power for dynamixel bus | None | None | dxlbus.power_off() |
scan() -> int |
Scan dynamixels, return the number of dynamixels found | None | 0 ~ 253 | dxlbus.scan() |
count() -> int |
Return the number of found dynamixel(s) | None | 0 ~ 253 | dxlbus.count() |
torque_on() -> None |
Turn on torque for all found dynamixel(s) | None | None | dxlbus.torque_on() |
torque_off() -> None |
Turn off torque for all found dynamixel(s) | None | None | dxlbus.torque_off() |
reboot() -> None |
Reboot all dynamixel(s) | None | None | dxlbus.reboot() |
Motion Submodule
| Methods of motion submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
speed() -> int |
Return motion speed (%) | None | 20% ~ 200% | motion.speed() |
speed(speed: int) -> int |
Set motion speed (%) | 20% ~ 200% | None | motion.speed(150) |
play(motion: int) -> None |
Play a specified motion page or stop current motion | 0 : Stop motion using an Exit Motion Unit 1~65532 : Play motion with a specified page 65533 : Stop motion immediately 65534 : Stop motion at the current Key Frame 65535 : Stop motion at current unit |
None | motion.play(1) |
play(motion: int, next: int) -> None |
Play a specified motion with a motion reserved for playing contiguously | motion0 : Stop motion using an Exit Motion Unit 1~65532 : Play motion with a specified page 65533 : Stop motion immediately 65534 : Stop motion at the current Key Frame 65535 : Stop motion at current unit next0~65534 : Page to move next. 65535 : No next page |
None | motion.play(1, 2) |
next(next: int) -> None |
Reserve the next motion to play contiguously. This function must be used before motion.play(motion) |
next0~65534 : Page to move next. 65535 : No next page |
None | motion.next(2) |
status() -> bool |
Return motion play status | None | True : Motion is being played False : Motion is NOT being played |
motion.status() |
count() -> int |
Return the number of motions stored in FLASH memory | None | 0 ~ 1023 | motion.count() |
wait() -> None |
Wait until current motion stops playing | None | None | motion.wait() |
Buzzer Submodule
| Methods of buzzer submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
melody(index) -> None |
Play the specified melody by index. | 0 ~ 25 | None | buzzer.melody(1) |
note(index) -> None |
Play the specified note by index for 0.3 sec | 0 ~ 51 | None | buzzer.note(1) |
note(index, ms) -> None |
Play the specified note by index for specified time length | index0 ~ 51 ms(unit: 0.1s)0 ~ 50 : 0 ~ 5.0s |
buzzer.note(1, 10) |
|
wait() -> None |
Wait until current melody or note ends | None | None | buzzer.wait() |
Mic Submodule
| Methods of mic submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
counted() -> int |
Return the final number of detected sound after the clapping finishes | None | 0 ~ 255 | mic.counted() |
counting() -> int |
Return the real-time number of detected sound while the clapping continues | None | 0 ~ 255 | mic.counting() |
clear() -> int |
Clear the final number of detected sound to zero | None | None | mic.clear() |
IMU Submodule
| Methods of imu submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
roll() -> int |
Return the roll value of CM-550 controller | None | -18000 ~ 18000 | imu.roll() |
pitch() -> int |
Return the pitch value of CM-550 controller | None | -9000 ~ 9000 | imu.pitch() |
yaw() -> int |
Return the yaw value of CM-550 controller | None | -9000 ~ 9000 | imu.yaw() |
gyro_x() -> int |
Return the Gyro X axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01degree/sec) | imu.gyro_x() |
gyro_y() -> int |
Return the Gyro Y axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01degree/sec) | imu.gyro_y() |
gyro_z() -> int |
Return the Gyro Z axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01degree/sec) | imu.gyro_z() |
accel_x() -> int |
Return the accelerometer X axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01G) | imu.accel_x() |
accel_y() -> int |
Return the accelerometer Y axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01G) | imu.accel_y() |
accel_z() -> int |
Return the accelerometer Z axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01G) | imu.accel_z() |
OLLO Submodule
| Methods of OLLO submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
OLLO(port, mode) -> object |
Create an object with Port Number and Device Mode | modeconst.OLLO_WHEEL_SPEED ( port: 1 ~ 2)const.OLLO_JOINT_POSITION ( port: 1 ~ 2)const.OLLO_JOINT_SPEED ( port: 1 ~ 2)const.OLLO_IR ( port: 1 ~ 2)const.OLLO_MOISTURE ( port: 1 ~ 2)const.OLLO_MOISTURE_TEMP ( port: 1 ~ 2)const.OLLO_RED_BRIGHTNESS ( port: 1 ~ 2)const.OLLO_BLUE_BRIGHTNESS ( port: 1 ~ 2)const.OLLO_DMS ( port: 1 ~ 5)const.OLLO_TOUCH ( port: 1 ~ 5)const.OLLO_LED ( port: 1 ~ 5)const.OLLO_USER ( port: 1 ~ 5)const.OLLO_TEMPERATURE ( port: 1 ~ 5)const.OLLO_MAGNET ( port: 1 ~ 5)const.OLLO_MOTION_DETECTION ( port: 1 ~ 5)const.OLLO_COLOR ( port: 1 ~ 5)const.OLLO_BRIGHTNESS ( port: 1 ~ 5) |
5-pin port object | obj = OLLO(1, OLLO_WHEEL_SPEED) |
read() -> int |
Return the value of object | None | 0 ~ 2047 (mode: const.OLLO_WHEEL_SPEED)0 ~ 1023 ( mode: const.OLLO_JOINT_POSITION)0 ~ 1023 ( mode: const.OLLO_JOINT_SPEED)0 ~ 1023 ( mode: const.OLLO_IR)0 ~ 100 ( mode: const.OLLO_MOISTURE, unit: %)-19 ~ 105 ( mode: const.OLLO_MOISTURE_TEMP, unit: ℃)0 ~ 100 ( mode: const.OLLO_RED_BRIGHTNESS, unit: %)0 ~ 100 ( mode: const.OLLO_BLUE_BRIGHTNESS, unit: %)0 ~ 1023 ( mode: const.OLLO_DMS)0, 1 ( mode: const.OLLO_TOUCH)0 ~ 3 ( mode: const.OLLO_LED)0 ~ 1023 ( mode: const.OLLO_USER)-20 ~ 120 ( mode: const.OLLO_TEMPERATURE, unit: ℃)0, 1 ( mode: const.OLLO_MAGNET)0 ~ 1 ( mode: const.OLLO_MOTION_DETECTION)0 ~ 6 ( mode: const.OLLO_COLOR)0 ~ 100 ( mode: const.OLLO_BRIGHTNESS, unit: %) |
obj.read() |
write(speed) -> None |
Set wheel speed of object of wheel mode ( mode: const.OLLO_WHEEL_SPEED) |
0 ~ 1023 : CCW (Counter clock wise) speed 1024 ~ 2047 : CW (Clockwise) speed |
None | obj.write(512) |
write(position) -> None |
Set joint poistion of object of joint mode ( mode: const.OLLO_JOINT_POSITION) |
0 ~ 1023 | None | obj.write(512) |
write(speed) -> None |
Set moving speed of object of joint mode ( mode: const.OLLO_JOINT_POSITION) |
0 ~ 1023 | None | obj.write(256) |
write(pwm) -> None |
Set pwm duty cycle of object of LED brightness mode ( mode: const.OLLO_RED_BRIGHTNESS / OLLO_BLUE_BRIGHTNESS) |
0 ~ 100 (unit: %) | None | obj.write(50) |
write(left, right) -> None |
Set LED status of left and right LED of LED module ( mode: const.OLLO_LED) |
0, 1 | None | obj.write(1, 0) |
write(left, right) -> None |
Set LED status of left and right output port of User Device ( mode: const.OLLO_USER) |
0, 1 | None | obj.write(1, 1) |
DXL Submodule
| Methods of DXL submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
DXL(id) -> object |
Create an Dynamixel object with specified ID | 0 ~ 252 : Single ID 254 : Broadcast ID |
Dynamixel object | obj = DXL(1) |
mode() -> int |
Return mode number of Dynamixel object | None | 1 : Velocity Control Mode 3 : Position Control Mode 4 : Multi-turn Mode |
obj.mode() |
mode(mode) -> None |
Set mode for Dynamixel object | 1 : Velocity Control Mode 3 : Position Control Mode 4 : Multi-turn Mode |
None | obj.mode(3) |
torque_on() -> None |
Turn on torque for Dynamixel object | None | None | obj.torque_on() |
torque_off() -> None |
Turn off torque for Dynamixel object | None | None | obj.torque_off() |
led_on() -> None |
Turn on LED for Dynamixel object | None | None | obj.led_on() |
led_off() -> None |
Turn off LED for Dynamixel object | None | None | obj.led_off() |
led_toggle() -> None |
Toggle LED for Dynamixel object | None | None | obj.led_toggle() |
goal_velocity() -> int |
Return goal velocity value | None | -1023 ~ 1023 (unit: 0.229 rev/min) | obj.goal_velocity() |
goal_velocity(v) -> None |
Set goal velocity value | -1023 ~ 1023 (unit: 0.229 rev/min) | None | obj.goal_velocity(100) |
goal_position() -> int |
Return goal position value | None | -4095 ~ 4095 | obj.goal_position() |
goal_position(p) -> None |
Set goal position value | -4095 ~ 4095 | None | obj.goal_position(1024) |
is_moving() -> bool |
Return moving status | None | True : Dynamixel is moving False : Dyanmixel is not moving |
obj.is_moving() |
present_velocity() -> int |
Return present velocity value | None | -1023 ~ 1023 (unit: 0.229 rev/min) | obj.present_velocity() |
present_position() -> int |
Return present position value | None | -4095 ~ 4095 | obj.present_position() |
RPI Submodule
| Methods of rpi submodule | Description | Parameter | Return | Example |
|---|---|---|---|---|
mode() -> int |
Return mode number of connected Raspberry Pi | None | 0 : Standby 1 : Color Detection 2 : Face Detection 3 : Streaming |
rpi.mode() |
mode(mode: int) -> None |
Set the mode of the connected Raspberry Pi | mode0 : Standby 1 : Color Detection 2 : Face Detection 3 : Streaming |
None | rpi.mode(1) |
sub_mode() -> int |
Return the sub-mode of the current mode (only for Color Detection Mode) |
None | 1 : Red 2 : Orange 3 : Yellow 4 : Green 5 : Blue 6 : Purple 7 : White |
rpi.sub_mode() |
sub_mode(mode: int) -> None |
Set the sub-mode of the current mode (only for Color Detection Mode) |
mode1 : Red 2 : Orange 3 : Yellow 4 : Green 5 : Blue 6 : Purple 7 : White |
None | rpi.sub_mode(1) |
ip() -> tuple |
Return the IP address of the connected Raspberry Pi as a tuple with 4 integers | None | IP address as a tuple eg. (192, 168, 13, 5) |
rpi.ip() |
position_x() -> int |
Return the x-coordinate of the camera detection position | None | X-coordinate value | rpi.position_x() |
position_y() -> int |
Return the y-coordinate of the camera detection position | None | Y-coordinate value | rpi.position_y() |
area() -> int |
Return the detection area of the camera | None | Area value | rpi.area() |
resolution_w() -> int |
Return the width of the camera resolution | None | Width in pixels | rpi.resolution_w() |
resolution_h() -> int |
Return the height of the camera resolution | None | Height in pixels | rpi.resolution_h() |
h_max() -> int |
Return the maximum hue value for color detection | None | 0 ~ 179 | rpi.h_max() |
h_max(h_max: int) -> None |
Set the maximum hue value for color detection | 0 ~ 179 | None | rpi.h_max(179) |
h_min() -> int |
Return the minimum hue value for color detection | None | 0 ~ 179 | rpi.h_min() |
h_min(h_min: int) -> None |
Set the minimum hue value for color detection | 0 ~ 179 | None | rpi.h_min(0) |
s_max() -> int |
Return the maximum saturation value for color detection | None | 0 ~ 255 | rpi.s_max() |
s_max(s_max: int) -> None |
Set the maximum saturation value for color detection | 0 ~ 255 | None | rpi.s_max(255) |
s_min() -> int |
Return the minimum saturation value for color detection | None | 0 ~ 255 | rpi.s_min() |
s_min(s_min: int) -> None |
Set the minimum saturation value for color detection | 0 ~ 255 | None | rpi.s_min(0) |
v_max() -> int |
Return the maximum value (brightness) for color detection | None | 0 ~ 255 | rpi.v_max() |
v_max(v_max: int) -> None |
Set the maximum value (brightness) for color detection | 0 ~ 255 | None | rpi.v_max(255) |
v_min() -> int |
Return the minimum value (brightness) for color detection | None | 0 ~ 255 | rpi.v_min() |
v_min(v_min: int) -> None |
Set the minimum value (brightness) for color detection | 0 ~ 255 | None | rpi.v_min(0) |