Edit on GitHub

Overview

ROS-enabled OpenMANIPULATOR-X (RM-X52-TNM) is a full open robot platform consisting of OpenSoftware​, OpenHardware and OpenCR(Embedded board)​.

OpenSoftware

OpenMANIPULATOR-X RM-X52-TNM are based on ROS ​and OpenSource. ROS official hardware platform,TurtleBot series has been supporting ‘TurtleBot Arm’. The OpenMANIPULATOR-X RM-X52-TNM has full hardware compatibility with TurtleBot3​. Users can also control it more easily by linking it with the MoveIt! package. Even if you do not have an actual robot, you can control the robot in the Gazebo simulator​.

OpenHardware

OpenMANIPULATOR-X RM-X52-TNM is an open-hardware oriented platform​. Most of the components are uploaded as STL files so that users can easily 3d print them. It also allows users to modify the length of the links or the design of the robot for their own purposes. OpenMANIPULATOR-X RM-X52-TNM is made of DYNAMIXEL-X ​Series which is used in TurtleBot 3.

OpenCR (Embedded board)

OpenMANIPULATOR-X RM-X52-TNM can also be controlled using OpenCR (Open-source Control module for ROS), the control board used in TurtleBot3. The computing power and real-time controllability of OpenCR can support forward and inverse kinematics, and profile control examples.

DYNAMIXEL Examples

OpenMANIPULATOR-X RM-X52-TNM is composed of DYNAMIXEL-X series and 3D printing parts. DYNAMIXEL has a modular form and adopts the daisy chain method. It allows users to easily add or remove joints for their own use. Taking advantage of this characteristic, users can build seven different types of OpenMANIPULATOR-X series : Chain, SCARA, Link, Planar, Delta, Stewart and Linear.

Introduction Video

ROSCon 2017 Vancouver Day 1: Introducing OpenMANIPULATOR; the full open robot platform from OSRF on Vimeo.