Library Setup <C++ Linux>
This section provides instructions on building the SDK.
Install requirements
- The DYNAMIXEL SDK requires GNU gcc ver. 5.4.0 20160609 or higher
- To check the version of your gcc compiler
$ gcc -v - Download the requirements
$ sudo apt-get install gcc $ sudo apt-get install build-essential $ sudo apt-get install gcc-multilib g++-multilib # For cross-compiling
Build the SDK
- Check your system architecture
$ uname -m - Enter the appropriate build folder depending on your system and build the SDK
$ cd DynamixelSDK/c++/build/linux64 # for 64-bit systems $ sudo make install - make sure to enter the correct folder according to your system architecture.
linux64for 64-bit systemslinux32for 32-bit systemslinux_sbcfor ARM-based SBCs like Raspberry Pi
- If the build completes successfully, you should see the .so file generated inside the build folder.
$ ls libdxl_x86_cpp.so Makefile - Grant permission to access the port
$ sudo chmod 666 /dev/ttyUSB0
- Common
makecommands for building the SDK$ make # Compile the source code and generate binaries $ make install # Install the library files to the system $ make clean # Remove all build files and reset the build environment $ make uninstall # Remove files installed by 'make install' from the system $ make reinstall # Reinstall by cleaning, rebuilding, and installing again
Library Setup <C++ Windows>
This section provides instructions on building the SDK.
Install requirements
-
In this section, we used visual studio as the IDE for building the SDK.
Download Visual Studio Community for Windows Desktop

Build the SDK
NOTE: This instruction assumes a 64-bit Windows system. If you are using 32-bit Windows, simply follow the same steps using the 32-bit version instead.
-
Open the project solution file (
dxl_x64_cpp.sln) located in the[DynamixelSDK folder]/c++/build/win64directory.
-
If below dialog appears, select
OK. This will adjust the toolset settings depending on your version of Visual Studio and Windows.
-
In the Solution Explorer on the right side, right-click the dxl_x64_cpp solution and select Build.

- The SDK build is complete.
- If the build was successful, the compiled library file will be saved at :
[DynamixelSDK folder]/c++/build/[win64]/output/dxl_x64_cpp.dll
Check Build Properties
-
You can check or change the build properties through right-clicking on the project in the Solution Explorer and selecting Properties.

-
Build properties is shown as below

- Output Directory:
$(SolutionDir)output\ - Intermediate Directory:
$(Configuration)\ - Platform Toolset:
Visual Studio 20XX (v000) - Configuration Type:
Dynamic Library (.dll)

- Additional Include Directories:
..\..\..\include\dynamixel_sdk
- Output Directory:
WARNING:
If the library file needs to be built in a lower or higher version of Visual Studio, change the Platform Toolset into the needed value. (ex: To use the DynamixelSDK c ver. library file in the MATLAB 2010 or LabVIEW 2010, the Platform Toolset should be changed to Visual Studio 2009 lower.)
Library Setup <C++ macOS>
Maintenance is in progress. We apologize for your inconvenience. The manual is available in the near future.