Edit on GitHub

Bulk Read/Write Tutorial <C++>

NOTE: This tutorial is based on XL-430-W250 DYNAMIXEL motors and uses Protocol 2.0.

This section provides examples of how to write code in C++ to bulk_read and bulk_write data to DYNAMIXEL motors.
Bulk Read/Write enables simultaneous control of multiple motors.
Unlike Sync Read/Write, which can only access the same address across multiple motors, Bulk Read/Write can access different addresses on multiple motors in a single instruction.
In this example, we need two motors to operate simultaneously.

Make cpp file

  • Create a CPP file and open it in a text editor. In this case, we use visual studio code, but you can use any text editor you prefer.
    $ mkdir -p my_dxl_project/src
    $ cd my_dxl_project/src
    $ code my_bulk_read_write.cpp
    
  • Open Visual Studio and create a new project as a Console Application.

Source Code Description

Add Header Files

Initialize Handler Objects

  • Make main function and initialize the PortHandler,PacketHandler,GroupBulkWrite and GroupBulkRead. Set the port name and protocol version according to your DYNAMIXEL setup. The example below uses /dev/ttyUSB0 as the port name and 2.0 as the protocol version.
    int main(){
      dynamixel::PortHandler *portHandler = dynamixel::PortHandler::getPortHandler("/dev/ttyUSB0"); // your dxl port name
      dynamixel::PacketHandler *packetHandler = dynamixel::PacketHandler::getPacketHandler(2.0); //protocol version
      dynamixel::GroupBulkWrite groupBulkWrite(portHandler, packetHandler);
      dynamixel::GroupBulkRead groupBulkRead(portHandler, packetHandler);
    
  • Make main function and initialize the PortHandler,PacketHandler,GroupBulkWrite and GroupBulkRead. Set the port name and protocol version according to your DYNAMIXEL setup. The example below uses COM3 as the port name and 2.0 as the protocol version.
    int main(){
      dynamixel::PortHandler *portHandler = dynamixel::PortHandler::getPortHandler("COM3"); // your dxl port name
      dynamixel::PacketHandler *packetHandler = dynamixel::PacketHandler::getPacketHandler(2.0); //protocol version
      dynamixel::GroupBulkWrite groupBulkWrite(portHandler, packetHandler);
      dynamixel::GroupBulkRead groupBulkRead(portHandler, packetHandler);
    

Open Port and Set Baud Rate

ERROR LOGGING

openPort() and setBaudRate() functions return a boolean value indicating success or failure. If you want to check for failure, you can write like below to print an error message and exit the program.

  if (portHandler->openPort()) {
    std::cout << "Succeeded to open the port!\n";
  } else {
    std::cout << "Failed to open the port!\n";
    return 0;
  }

  if (portHandler->setBaudRate(57600)) {
    std::cout << "Succeeded to change the baudrate!\n";
  } else {
    std::cout << "Failed to change the baudrate!\n";
    return 0;
  }

Write data to enable torque

ERROR LOGGING

write1ByteTxRx() returns a communication result. If you want to check the communication result and error, you can write the code as shown below.
The dxl_comm_result, dxl_error variable should be declared beforehand.

  uint8_t dxl_error = 0;
  int dxl_comm_result = COMM_TX_FAIL;  //COMM_TX_FAIL is a constant defined in the SDK
  ...
  dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id1, torque_on_address, data, &dxl_error);
  if (dxl_comm_result != COMM_SUCCESS) {
    std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
  } else if (dxl_error != 0) {
    std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
  } else {
    std::cout << "Dynamixel#1 has been successfully connected \n";
  }

  dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id2, torque_on_address, data, &dxl_error);
  if (dxl_comm_result != COMM_SUCCESS) {
    std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
  } else if (dxl_error != 0) {
    std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
  } else {
    std::cout << "Dynamixel#2 has been successfully connected \n";
  }

Add Parameters to GroupBulkRead

ERROR LOGGING

addParam() returns a communication result as boolean. If you want to check the communication result and error, you can write the code as shown below.
The dxl_addparam_result variable should be declared beforehand.

  bool dxl_addparam_result = false;
  dxl_addparam_result = groupBulkRead.addParam(dxl_id1, present_position_address, data_length_4byte);
  if (!dxl_addparam_result) {
    std::cout <<"[ID:" << (int)dxl_id1  <<"]groupBulkRead addparam failed" << std::endl;
    return 0;
  }

  dxl_addparam_result = groupBulkRead.addParam(dxl_id2, led_address, data_length_1byte);
  if (!dxl_addparam_result) {
    std::cout <<"[ID:" << (int)dxl_id2  <<"]groupBulkRead addparam failed" << std::endl;
    return 0;
  }

Get User Input and Set Data

Add parameter to GroupBulkWrite and Write Data

ERROR LOGGING

txPacket() and addParam() returns a communication result. If you want to check the communication result and error, you can write the code as shown below.
The dxl_addparam_result, dxl_comm_result variables should be declared beforehand.

  bool dxl_addparam_result = false;
  int dxl_comm_result = COMM_TX_FAIL;  //COMM_TX_FAIL is a constant defined in the SDK
    dxl_addparam_result = groupBulkWrite.addParam(dxl_id1, goal_position_address, data_length_4byte, param_goal_position);
    if (!dxl_addparam_result) {
      std::cout <<"[ID:" << (int)dxl_id1  <<"]groupBulkWrite addparam failed" << std::endl;
      return 0;
    }

    dxl_addparam_result = groupBulkWrite.addParam(dxl_id2, led_address, data_length_1byte, &led_data);
    if (!dxl_addparam_result) {
      std::cout <<"[ID:" << (int)dxl_id2  <<"]groupBulkWrite addparam failed" << std::endl;
      return 0;
    }

    dxl_comm_result = groupBulkWrite.txPacket();
    if (dxl_comm_result != COMM_SUCCESS) {
      std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
    }

Read data from DYNAMIXEL

ERROR LOGGING

txRxPacket() and isAvailable() returns a communication result . If you want to check the communication result and error, you can write the code as shown below.
The dxl_getdata_result, dxl_comm_result variables should be declared beforehand.

  bool dxl_getdata_result = false;
  int dxl_comm_result = COMM_TX_FAIL;  //COMM_TX_FAIL is a constant defined in the SDK
      dxl_comm_result = groupBulkRead.txRxPacket();
      if (dxl_comm_result != COMM_SUCCESS) {
        std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
      }

You can also check if the data is available in the GroupBulkRead by using the isAvailable() function. If the data is not available, you can print an error message and exit the program.

      dxl_getdata_result = groupBulkRead.isAvailable(dxl_id1, present_position_address, data_length_4byte);
      if (dxl_getdata_result != true) {
        std::cout << "[ID:" << (int)dxl_id1 << "] groupBulkRead getdata failed" << std::endl;
        return 0;
      }

      dxl_getdata_result = groupBulkRead.isAvailable(dxl_id2, led_address, data_length_1byte);
      if (dxl_getdata_result != true) {
        std::cout << "[ID:" << (int)dxl_id2 << "] groupBulkRead getdata failed" << std::endl;
        return 0;
      }

Compile and Run

  • Compile the code using g++.
    $ g++ my_bulk_read_write.cpp -o my_bulk_read_write -ldxl_x64_cpp
    $ ./my_bulk_read_write
    
  • Set build properties.

    • C/C++ → Additional Include Directories : {$Dynamixel_SDK_PATH\c++\include}
    • Debugging → Environment : PATH=%PATH%;{$Dynamixel_SDK_PATH\c++\build\win64\output} (if you use 32bit architecture, use {$Dynamixel_SDK_PATH\c++\build\win32\output})

    • Linker → Additional Library Directories : {$Dynamixel_SDK_PATH\c++\build\win64\output} (if you use 32bit architecture, use {$Dynamixel_SDK_PATH\c++\build\win32\output})
    • Linker → Input → Additional Dependencies : dxl_x64_cpp.lib


  • Build properties setup is complete. You can now build and run the project.

  • After building, you can find the executable file( .exe ) in the output directory : {$YOUR_SLN_DIR\x64\}

WARNING: If you execute the .exe file directly(not through the IDE), you might encounter a missing DLL error. To fix this, ensure that dxl_x64_cpp.dll is either in your system PATH or in the same directory as the application.

Full Source Code

#include "dynamixel_sdk/dynamixel_sdk.h"
#include <iostream>

int main(){
  dynamixel::PortHandler *portHandler = dynamixel::PortHandler::getPortHandler("/dev/ttyUSB0");
  dynamixel::PacketHandler *packetHandler = dynamixel::PacketHandler::getPacketHandler(2.0);
  dynamixel::GroupBulkWrite groupBulkWrite(portHandler, packetHandler);
  dynamixel::GroupBulkRead groupBulkRead(portHandler, packetHandler);

  uint8_t dxl_error = 0;
  int dxl_comm_result = COMM_TX_FAIL;
  bool dxl_addparam_result = false;
  bool dxl_getdata_result = false;

  if (portHandler->openPort()) {
    std::cout << "Succeeded to open the port!\n";
  } else {
    std::cout << "Failed to open the port!\n";
    return 0;
  }

  if (portHandler->setBaudRate(57600)) {
    std::cout << "Succeeded to change the baudrate!\n";
  } else {
    std::cout << "Failed to change the baudrate!\n";
    return 0;
  }

  uint8_t dxl_id1 = 1;
  uint8_t dxl_id2 = 2;
  uint16_t torque_on_address = 64;
  uint8_t data = 1;
  dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id1, torque_on_address, data, &dxl_error);
  if (dxl_comm_result != COMM_SUCCESS) {
    std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
  } else if (dxl_error != 0) {
    std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
  } else {
    std::cout << "Dynamixel#1 has been successfully connected \n";
  }

  dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id2, torque_on_address, data, &dxl_error);
  if (dxl_comm_result != COMM_SUCCESS) {
    std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
  } else if (dxl_error != 0) {
    std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
  } else {
    std::cout << "Dynamixel#2 has been successfully connected \n";
  }

  uint16_t present_position_address = 132;
  uint16_t data_length_4byte = 4;
  dxl_addparam_result = groupBulkRead.addParam(dxl_id1, present_position_address, data_length_4byte);
  if (!dxl_addparam_result) {
    std::cout <<"[ID:" << (int)dxl_id1  <<"]groupBulkRead addparam failed" << std::endl;
    return 0;
  }

  uint16_t led_address = 65;
  uint16_t data_length_1byte = 1;
  dxl_addparam_result = groupBulkRead.addParam(dxl_id2, led_address, data_length_1byte);
  if (!dxl_addparam_result) {
    std::cout <<"[ID:" << (int)dxl_id2  <<"]groupBulkRead addparam failed" << std::endl;
    return 0;
  }

  int target_position = 0;
  uint8_t dxl2_led_value_read = 0;
  while(true){
    std::cout << "Enter target position (0 ~ 4095): ";
    std::cin >> target_position;
    if(target_position == -1){
      break;
    } else if(target_position < 0 || target_position > 4095){
      std::cout << "Position must be between 0 and 4095." << std::endl;
      continue;
    }

    uint8_t param_goal_position[4];
    param_goal_position[0] = DXL_LOBYTE(DXL_LOWORD(target_position));
    param_goal_position[1] = DXL_HIBYTE(DXL_LOWORD(target_position));
    param_goal_position[2] = DXL_LOBYTE(DXL_HIWORD(target_position));
    param_goal_position[3] = DXL_HIBYTE(DXL_HIWORD(target_position));

    uint8_t led_data = 0;
    if (dxl2_led_value_read == 0){
      led_data = 1;
    } else {
      led_data = 0;
    }

    uint16_t goal_position_address = 116;
    dxl_addparam_result = groupBulkWrite.addParam(dxl_id1, goal_position_address, data_length_4byte, param_goal_position);
    if (!dxl_addparam_result) {
      std::cout <<"[ID:" << (int)dxl_id1  <<"]groupBulkWrite addparam failed" << std::endl;
      return 0;
    }

    dxl_addparam_result = groupBulkWrite.addParam(dxl_id2, led_address, data_length_1byte, &led_data);
    if (!dxl_addparam_result) {
      std::cout <<"[ID:" << (int)dxl_id2  <<"]groupBulkWrite addparam failed" << std::endl;
      return 0;
    }

    dxl_comm_result = groupBulkWrite.txPacket();
    if (dxl_comm_result != COMM_SUCCESS) {
      std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
    }
    groupBulkWrite.clearParam();

    int dxl1_present_position;
    do{
      dxl_comm_result = groupBulkRead.txRxPacket();
      if (dxl_comm_result != COMM_SUCCESS) {
        std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
      }
      dxl_getdata_result = groupBulkRead.isAvailable(dxl_id1, present_position_address, data_length_4byte);
      if (dxl_getdata_result != true) {
        std::cout << "[ID:" << (int)dxl_id1 << "] groupBulkRead getdata failed" << std::endl;
        return 0;
      }

      dxl_getdata_result = groupBulkRead.isAvailable(dxl_id2, led_address, data_length_1byte);
      if (dxl_getdata_result != true) {
        std::cout << "[ID:" << (int)dxl_id2 << "] groupBulkRead getdata failed" << std::endl;
        return 0;
      }
      dxl1_present_position = groupBulkRead.getData(dxl_id1, present_position_address, data_length_4byte);
      dxl2_led_value_read = groupBulkRead.getData(dxl_id2, led_address, data_length_1byte);
      printf("[ID:%03d] Present Position : %d \t [ID:%03d] LED Value: %d\n", dxl_id1, dxl1_present_position, dxl_id2, dxl2_led_value_read);
    } while (abs(target_position - dxl1_present_position) > 10);
  }
  data = 0;
  packetHandler->write1ByteTxRx(portHandler, dxl_id1, torque_on_address, data);
  packetHandler->write1ByteTxRx(portHandler, dxl_id2, torque_on_address, data);
  portHandler->closePort();

  return 0;
}
#include "dynamixel_sdk/dynamixel_sdk.h"
#include <iostream>

int main(){
  dynamixel::PortHandler *portHandler = dynamixel::PortHandler::getPortHandler("COM3");
  dynamixel::PacketHandler *packetHandler = dynamixel::PacketHandler::getPacketHandler(2.0);
  dynamixel::GroupBulkWrite groupBulkWrite(portHandler, packetHandler);
  dynamixel::GroupBulkRead groupBulkRead(portHandler, packetHandler);

  uint8_t dxl_error = 0;
  int dxl_comm_result = COMM_TX_FAIL;
  bool dxl_addparam_result = false;
  bool dxl_getdata_result = false;

  if (portHandler->openPort()) {
    std::cout << "Succeeded to open the port!\n";
  } else {
    std::cout << "Failed to open the port!\n";
    return 0;
  }

  if (portHandler->setBaudRate(57600)) {
    std::cout << "Succeeded to change the baudrate!\n";
  } else {
    std::cout << "Failed to change the baudrate!\n";
    return 0;
  }

  uint8_t dxl_id1 = 1;
  uint8_t dxl_id2 = 2;
  uint16_t torque_on_address = 64;
  uint8_t data = 1;
  dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id1, torque_on_address, data, &dxl_error);
  if (dxl_comm_result != COMM_SUCCESS) {
    std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
  } else if (dxl_error != 0) {
    std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
  } else {
    std::cout << "Dynamixel#1 has been successfully connected \n";
  }

  dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id2, torque_on_address, data, &dxl_error);
  if (dxl_comm_result != COMM_SUCCESS) {
    std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
  } else if (dxl_error != 0) {
    std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
  } else {
    std::cout << "Dynamixel#2 has been successfully connected \n";
  }

  uint16_t present_position_address = 132;
  uint16_t data_length_4byte = 4;
  dxl_addparam_result = groupBulkRead.addParam(dxl_id1, present_position_address, data_length_4byte);
  if (!dxl_addparam_result) {
    std::cout <<"[ID:" << (int)dxl_id1  <<"]groupBulkRead addparam failed" << std::endl;
    return 0;
  }

  uint16_t led_address = 65;
  uint16_t data_length_1byte = 1;
  dxl_addparam_result = groupBulkRead.addParam(dxl_id2, led_address, data_length_1byte);
  if (!dxl_addparam_result) {
    std::cout <<"[ID:" << (int)dxl_id2  <<"]groupBulkRead addparam failed" << std::endl;
    return 0;
  }

  int target_position = 0;
  uint8_t dxl2_led_value_read = 0;
  while(true){
    std::cout << "Enter target position (0 ~ 4095): ";
    std::cin >> target_position;
    if(target_position == -1){
      break;
    } else if(target_position < 0 || target_position > 4095){
      std::cout << "Position must be between 0 and 4095." << std::endl;
      continue;
    }

    uint8_t param_goal_position[4];
    param_goal_position[0] = DXL_LOBYTE(DXL_LOWORD(target_position));
    param_goal_position[1] = DXL_HIBYTE(DXL_LOWORD(target_position));
    param_goal_position[2] = DXL_LOBYTE(DXL_HIWORD(target_position));
    param_goal_position[3] = DXL_HIBYTE(DXL_HIWORD(target_position));

    uint8_t led_data = 0;
    if (dxl2_led_value_read == 0){
      led_data = 1;
    } else {
      led_data = 0;
    }

    uint16_t goal_position_address = 116;
    dxl_addparam_result = groupBulkWrite.addParam(dxl_id1, goal_position_address, data_length_4byte, param_goal_position);
    if (!dxl_addparam_result) {
      std::cout <<"[ID:" << (int)dxl_id1  <<"]groupBulkWrite addparam failed" << std::endl;
      return 0;
    }

    dxl_addparam_result = groupBulkWrite.addParam(dxl_id2, led_address, data_length_1byte, &led_data);
    if (!dxl_addparam_result) {
      std::cout <<"[ID:" << (int)dxl_id2  <<"]groupBulkWrite addparam failed" << std::endl;
      return 0;
    }

    dxl_comm_result = groupBulkWrite.txPacket();
    if (dxl_comm_result != COMM_SUCCESS) {
      std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
    }
    groupBulkWrite.clearParam();

    int dxl1_present_position;
    do{
      dxl_comm_result = groupBulkRead.txRxPacket();
      if (dxl_comm_result != COMM_SUCCESS) {
        std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
      }
      dxl_getdata_result = groupBulkRead.isAvailable(dxl_id1, present_position_address, data_length_4byte);
      if (dxl_getdata_result != true) {
        std::cout << "[ID:" << (int)dxl_id1 << "] groupBulkRead getdata failed" << std::endl;
        return 0;
      }

      dxl_getdata_result = groupBulkRead.isAvailable(dxl_id2, led_address, data_length_1byte);
      if (dxl_getdata_result != true) {
        std::cout << "[ID:" << (int)dxl_id2 << "] groupBulkRead getdata failed" << std::endl;
        return 0;
      }
      dxl1_present_position = groupBulkRead.getData(dxl_id1, present_position_address, data_length_4byte);
      dxl2_led_value_read = groupBulkRead.getData(dxl_id2, led_address, data_length_1byte);
      printf("[ID:%03d] Present Position : %d \t [ID:%03d] LED Value: %d\n", dxl_id1, dxl1_present_position, dxl_id2, dxl2_led_value_read);
    } while (abs(target_position - dxl1_present_position) > 10);
  }
  data = 0;
  packetHandler->write1ByteTxRx(portHandler, dxl_id1, torque_on_address, data);
  packetHandler->write1ByteTxRx(portHandler, dxl_id2, torque_on_address, data);
  portHandler->closePort();

  return 0;
}