CPP GroupBulkRead
-
Description
Base class for simultaneous dynamixel control on writing.
-
Members
None
-
Methods
Methods | Description |
---|---|
GroupBulkRead | Initializes groupBulkRead instance |
~GroupBulkRead | Clears parameter storage |
getPortHandler | Returns PortHandler instance |
getPacketHandler | Returns PacketHandler instance |
addParam | Adds parameter storage for read |
removeParam | Removes parameter on the storage |
clearParam | Clears parameter storage |
txPacket | Transmits packet to the number of Dynamixels |
rxPacket | receives packet from the number of Dynamixels |
txRxPacket | Transmits and receives packet on the number of Dynamixels |
isAvailable | Checks whether there is available data in the data storage |
getData | Gets data from received packet |
-
Enumerator
None
Method References
addParam
- Syntax
bool addParam(uint8_t id, uint16_t start_address, uint16_t data_length)
- Parameters
Parameters | Description | |
---|---|---|
id | Dynamixel ID | |
start_address | Address on the control table of Dynamixel | |
data_length | data_length |
-
Detailed Description
This function pushes
id
,start_address
,data_length
to the list, and initializes the parameter storage. It returns false when target ID exists already in the ID list, or returns true.
removeParam
- Syntax
void removeParam(UINT8_T id)
- Parameters
Parameters | Description |
---|---|
id | Dynamixel ID |
-
Detailed Description
This function removes target id in the Dynamixel ID list.
clearParam
- Syntax
void clearParam()
-
Parameters
None
-
Detailed Description
This function clears the Dynamixel ID list.
txPacket
- Syntax
int txPacket()
-
Parameters
None
-
Detailed Description
This function transmits the packet by using
syncReadTx
function. It returns communication result.
rxPacket
- Syntax
int rxPacket()
-
Parameters
None
-
Detailed Description
This function receives the packet by using
readRx
function. It returnsCOMM_NOT_AVAILABLE
when there is no packet that had been received, or returns communication result.
txRxPacket
- Syntax
int txRxPacket()
-
Parameters
None
-
Detailed Description
This function transmits and receives the packet by using
txPacket()
function andrxPacket()
function. It returnsCOMM_NOT_AVAILABLE
when the packet transmission had not succeeded, or returns communication result.
isAvailable
- Syntax ``` cpp bool isAvailable(uint8_t id, uint16_t address, uint16_t data_length)
- Parameters
| Parameters | Description |
|:-----------|:------------------------------------------|
| id | Dynamixel ID |
| address | Address on the control table of Dynamixel |
| data | Packet data |
- Detailed Description
This function checks whether there is available data in the data. It returns false when there is no data from target address, or returns true.
##### getData
- Syntax
``` cpp
uint32_t getData(uint8_t id, uint16_t address, uint16_t data_length)
- Parameters
Parameters | Description |
---|---|
id | Dynamixel ID |
address | Address on the control table of Dynamixel |
data_length | data length |
-
Detailed Description
This function gets specific data from received packet. It returns value.