Java GroupSyncWrite
-
Description
Base functions for simultaneous dynamixel control on writing to same length data on same control table address.
-
Members
None
-
Methods
Methods | Description |
---|---|
groupSyncWrite | Initializes members of packet data pointer struct |
groupSyncWriteAddParam | Adds parameter storage for read |
groupSyncWriteRemoveParam | Removes parameter on the storage |
groupSyncWriteChangeParam | Changes parameter on the storage |
groupSyncWriteClearParam | Clears parameter storage |
groupSyncWriteTxPacket | Transmits packet to the number of Dynamixels |
-
Enumerator
None
Method References
groupSyncWrite
- Syntax
int groupSyncWrite(int port_num, int protocol_version, short start_address, short data_length)
- Parameters
Parameters | Description |
---|---|
port_num | Port number |
protocol_version | Protocol version |
start_address | Control table address to start writing data |
data_length | Total data length |
-
Detailed Description
This function initializes the parameters for packet construction. The function resizes groupData struct and initialzes struct members.
groupSyncWriteAddParam
- Syntax
Boolean groupSyncWriteAddParam(int group_num, byte id, int data, short input_length)
- Parameters
Parameters | Description |
---|---|
group_num | Group number |
id | Dynamixel ID |
data | Data for write |
input_length | Input data length |
-
Detailed Description
This function pushes
id
to the Dynamixel ID list, and initializes #group_num
parameter storage by addinginput_length
bytesdata
. The function deals with 1, 2 or 4 byte data only. The function returns false when the length of input data exceeds parameter or wrong length, or returns true.
groupSyncWriteRemoveParam
- Syntax
void groupSyncWriteRemoveParam(int group_num, byte id)
- Parameters
Parameters | Description |
---|---|
group_num | Group number |
id | Dynamixel ID |
-
Detailed Description
This function removes
id
and its data for write in the #group_num
Dynamixel ID list. The function returns false when no data is in the parameter storage, or returns true.
groupSyncWriteChangeParam
- Syntax
Boolean groupSyncWriteChangeParam(int group_num, byte id, int data, short input_length, short data_pos)
- Parameters
Parameters | Description |
---|---|
group_num | Group number |
id | Dynamixel ID |
data | Data for write |
input_length | Input data length |
data_pos | Data position in the array |
-
Detailed Description
This function pushes new
data_length
bytesdata
into #group_num
parameter storage of sameid
. The function returns false when the target ID doesn’t exists in the ID list, or returns true.
groupSyncWriteClearParam
- Syntax
void groupSyncWriteClearParam(int group_num)
-
Parameters
None
-
Detailed Description
This function clears #
group_num
Dynamixel ID list.
groupSyncWriteTxPacket
- Syntax
void groupSyncWriteTxPacket(int group_num)
- Parameters
Parameters | Description |
---|---|
group_num | Group number |
-
Detailed Description
This function transmits the packet by using
syncWriteTxOnly
function. The communication result and the hardware error are available when the function is terminated.