Edit on GitHub

CPP DXL Monitor

Sample code

/*
 * dxl_monitor.cpp
 *
 *  Created on: 2016. 2. 21.
 *      Author: leon
 */

//
// *********     DXL Monitor Example      *********
//
//
// Available Dynamixel model on this example : All models using Protocol 1.0 and 2.0
// This example is tested with a Dynamixel MX-28, a Dynamixel PRO 54-200 and an USB2DYNAMIXEL
// To use another Dynamixel model, such as X series, see their details in E-Manual(support.robotis.com) and edit below "#define"d variables yourself.
// Be sure that properties of Dynamixel MX and PRO are already set as %% MX - ID : 1 / Baudnum : 1 (Baudrate : 1000000 [1M]) , PRO - ID : 1 / Baudnum : 3 (Baudrate : 1000000 [1M])
//

#ifdef __linux__
#include <unistd.h>
#include <fcntl.h>
#include <getopt.h>
#include <termios.h>
#elif defined(_WIN32) || defined(_WIN64)
#include <conio.h>
#endif

#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <vector>

#include "dynamixel_sdk.h"                                  // Uses Dynamixel SDK library

// Protocol version
#define PROTOCOL_VERSION1               1.0                 // See which protocol version is used in the Dynamixel
#define PROTOCOL_VERSION2               2.0

// Default setting
#define DEVICENAME                      "/dev/ttyUSB0"      // Check which port is being used on your controller
                                                            // ex) Windows: "COM1"   Linux: "/dev/ttyUSB0"

int getch()
{
#ifdef __linux__
  struct termios oldt, newt;
  int ch;
  tcgetattr(STDIN_FILENO, &oldt);
  newt = oldt;
  newt.c_lflag &= ~(ICANON | ECHO);
  tcsetattr(STDIN_FILENO, TCSANOW, &newt);
  ch = getchar();
  tcsetattr(STDIN_FILENO, TCSANOW, &oldt);
  return ch;
#elif defined(_WIN32) || defined(_WIN64)
  return _getch();
#endif
}

int kbhit(void)
{
#ifdef __linux__
  struct termios oldt, newt;
  int ch;
  int oldf;

  tcgetattr(STDIN_FILENO, &oldt);
  newt = oldt;
  newt.c_lflag &= ~(ICANON | ECHO);
  tcsetattr(STDIN_FILENO, TCSANOW, &newt);
  oldf = fcntl(STDIN_FILENO, F_GETFL, 0);
  fcntl(STDIN_FILENO, F_SETFL, oldf | O_NONBLOCK);

  ch = getchar();

  tcsetattr(STDIN_FILENO, TCSANOW, &oldt);
  fcntl(STDIN_FILENO, F_SETFL, oldf);

  if (ch != EOF)
  {
    ungetc(ch, stdin);
    return 1;
  }

  return 0;
#elif defined(_WIN32) || defined(_WIN64)
  return _kbhit();
#endif
}

void Usage(char *progname)
{
  printf("-----------------------------------------------------------------------\n");
  printf("Usage: %s\n");
  printf(" [-h | --help]........: display this help\n");
  printf("[-d | --device]......: port to open\n", progname);
  printf("-----------------------------------------------------------------------\n");
}

void Help()
{
  printf("\n");
  printf("                    .----------------------------.\n");
  printf("                    |  DXL Monitor Command List  |\n");
  printf("                    '----------------------------'\n");
  printf(" =========================== Common Commands ===========================\n");
  printf(" \n");
  printf(" help|h|?                    :Displays help information\n");
  printf(" baud [BAUD_RATE]            :Changes baudrate to [BAUD_RATE] \n");
  printf("                               ex) baud 2400 (2400 bps) \n");
  printf("                               ex) baud 1000000 (1 Mbps)  \n");
  printf(" exit                        :Exit this program\n");
  printf(" scan                        :Outputs the current status of all Dynamixels\n");
  printf(" ping [ID] [ID] ...          :Outputs the current status of [ID]s \n");
  printf(" bp                          :Broadcast ping (Dynamixel Protocol 2.0 only)\n");
  printf(" \n");
  printf(" ==================== Commands for Dynamixel Protocol 1.0 ====================\n");
  printf(" \n");
  printf(" wrb1|w1 [ID] [ADDR] [VALUE] :Write byte [VALUE] to [ADDR] of [ID]\n");
  printf(" wrw1 [ID] [ADDR] [VALUE]    :Write word [VALUE] to [ADDR] of [ID]\n");
  printf(" rdb1 [ID] [ADDR]            :Read byte value from [ADDR] of [ID]\n");
  printf(" rdw1 [ID] [ADDR]            :Read word value from [ADDR] of [ID]\n");
  printf(" r1 [ID] [ADDR] [LENGTH]     :Dumps the control table of [ID]\n");
  printf("                               ([LENGTH] bytes from [ADDR])\n");
  printf(" reset1|rst1 [ID]            :Factory reset the Dynamixel of [ID]\n");
  printf(" \n");
  printf(" ==================== Commands for Dynamixel Protocol 2.0 ====================\n");
  printf(" \n");
  printf(" wrb2|w2 [ID] [ADDR] [VALUE] :Write byte [VALUE] to [ADDR] of [ID]\n");
  printf(" wrw2 [ID] [ADDR] [VALUE]    :Write word [VALUE] to [ADDR] of [ID]\n");
  printf(" wrd2 [ID] [ADDR] [VALUE]    :Write dword [VALUE] to [ADDR] of [ID]\n");
  printf(" rdb2 [ID] [ADDR]            :Read byte value from [ADDR] of [ID]\n");
  printf(" rdw2 [ID] [ADDR]            :Read word value from [ADDR] of [ID]\n");
  printf(" rdd2 [ID] [ADDR]            :Read dword value from [ADDR] of [ID]\n");
  printf(" r2 [ID] [ADDR] [LENGTH]     :Dumps the control table of [ID]\n");
  printf("                               ([LENGTH] bytes from [ADDR])\n");
  printf(" reboot2|rbt2 [ID]           :reboot the Dynamixel of [ID]\n");
  printf(" reset2|rst2 [ID] [OPTION]   :Factory reset the Dynamixel of [ID]\n");
  printf("                               OPTION: 255(All), 1(Except ID), 2(Except ID&Baud)\n");

  printf("\n");
}

void Scan(dynamixel::PortHandler *portHandler, dynamixel::PacketHandler *packetHandler1, dynamixel::PacketHandler *packetHandler2)
{
  uint8_t dxl_error;
  uint16_t dxl_model_num;

  fprintf(stderr, "\n");
  fprintf(stderr, "Scan Dynamixel Using Protocol 1.0\n");
  for (int id = 1; id < 253; id++)
  {
    if (packetHandler1-> ping(portHandler, id, &dxl_model_num, &dxl_error)== COMM_SUCCESS)
    {
      fprintf(stderr, "\n                                          ... SUCCESS \r");
      fprintf(stderr, " [ID:%.3d] Model No : %.5d \n", id, dxl_model_num);
    }
    else
        fprintf(stderr, ".");

    if (kbhit())
    {
        char c = getch();
        if (c == 0x1b)
        break;
    }
  }
  fprintf(stderr, "\n\n");

  fprintf(stderr, "Scan Dynamixel Using Protocol 2.0\n");
  for (int id = 1; id < 253; id++)
  {
    if (packetHandler2-> ping(portHandler, id, &dxl_model_num, &dxl_error)== COMM_SUCCESS)
    {
      fprintf(stderr, "\n                                          ... SUCCESS \r");
      fprintf(stderr, " [ID:%.3d] Model No : %.5d \n", id, dxl_model_num);
    }
    else
    {
      fprintf(stderr, ".");
    }

    if (kbhit())
    {
      char c = getch();
      if (c == 0x1b) break;
    }
  }
  fprintf(stderr, "\n\n");
}

void Write(dynamixel::PortHandler *portHandler, dynamixel::PacketHandler *packetHandler, uint8_t id, uint16_t addr, uint16_t length, uint32_t value)
{
  uint8_t dxl_error = 0;
  int dxl_comm_result = COMM_TX_FAIL;

  if (length == 1)
  {
    dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, id, addr, (uint8_t)value, &dxl_error);
  }
  else if (length == 2)
  {
    dxl_comm_result = packetHandler->write2ByteTxRx(portHandler, id, addr, (uint16_t)value, &dxl_error);
  }
  else if (length == 4)
  {
    dxl_comm_result = packetHandler->write4ByteTxRx(portHandler, id, addr, (uint32_t)value, &dxl_error);
  }

  if (dxl_comm_result == COMM_SUCCESS)
  {
    if (dxl_error != 0) packetHandler->printRxPacketError(dxl_error);
    fprintf(stderr, "\n Success to write\n\n");
  }
  else
  {
    packetHandler->printTxRxResult(dxl_comm_result);
    fprintf(stderr, "\n Fail to write! \n\n");
  }
}

void Read(dynamixel::PortHandler *portHandler, dynamixel::PacketHandler *packetHandler, uint8_t id, uint16_t addr, uint16_t length)
{
  uint8_t dxl_error = 0;
  int     dxl_comm_result = COMM_TX_FAIL;

  int8_t  value8    = 0;
  int16_t value16   = 0;
  int32_t value32   = 0;


  if (length == 1)
  {
    dxl_comm_result = packetHandler->read1ByteTxRx(portHandler, id, addr, (uint8_t*)&value8, &dxl_error);
  }
  else if (length == 2)
  {
    dxl_comm_result = packetHandler->read2ByteTxRx(portHandler, id, addr, (uint16_t*)&value16, &dxl_error);
  }
  else if (length == 4)
  {
    dxl_comm_result = packetHandler->read4ByteTxRx(portHandler, id, addr, (uint32_t*)&value32, &dxl_error);
  }

  if (dxl_comm_result == COMM_SUCCESS)
  {
    if (dxl_error != 0) packetHandler->printRxPacketError(dxl_error);

    if (length == 1)
    {
      fprintf(stderr, "\n READ VALUE : (UNSIGNED) %u , (SIGNED) %d \n\n", (uint8_t)value8, value8);
    }
    else if (length == 2)
    {
      fprintf(stderr, "\n READ VALUE : (UNSIGNED) %u , (SIGNED) %d \n\n", (uint16_t)value16, value16);
    }
    else if (length == 4)
    {
      fprintf(stderr, "\n READ VALUE : (UNSIGNED) %u , (SIGNED) %d \n\n", (uint32_t)value32, value32);
    }
  }
  else
  {
    packetHandler->printTxRxResult(dxl_comm_result);
    fprintf(stderr, "\n Fail to read! \n\n");
  }
}

void Dump(dynamixel::PortHandler *portHandler, dynamixel::PacketHandler *packetHandler, uint8_t id, uint16_t addr, uint16_t len)
{
  uint8_t  dxl_error       = 0;
  int      dxl_comm_result = COMM_TX_FAIL;
  uint8_t *data            = (uint8_t*)calloc(len, sizeof(uint8_t));

  dxl_comm_result = packetHandler->readTxRx(portHandler, id, addr, len, data, &dxl_error);
  if (dxl_comm_result == COMM_SUCCESS)
  {
    if (dxl_error != 0)
      packetHandler->printRxPacketError(dxl_error);

    if (id != BROADCAST_ID)
    {
      fprintf(stderr, "\n");
      for (int i = addr; i < addr+len; i++)
      fprintf(stderr, "ADDR %.3d [0x%.4X] :     %.3d [0x%.2X] \n", i, i, data[i-addr], data[i-addr]);
      fprintf(stderr, "\n");
    }
  }
  else
  {
    packetHandler->printTxRxResult(dxl_comm_result);
    fprintf(stderr, "\n Fail to read! \n\n");
  }

  free(data);
}

int main(int argc, char *argv[])
{
  // Initialize Packethandler1 instance
  dynamixel::PacketHandler *packetHandler1 = dynamixel::PacketHandler::getPacketHandler(PROTOCOL_VERSION1);

  // Initialize Packethandler2 instance
  dynamixel::PacketHandler *packetHandler2 = dynamixel::PacketHandler::getPacketHandler(PROTOCOL_VERSION2);

  fprintf(stderr, "\n***********************************************************************\n");
  fprintf(stderr,   "*                            DXL Monitor                              *\n");
  fprintf(stderr,   "***********************************************************************\n\n");

  char *dev_name = (char*)DEVICENAME;

#ifdef __linux__
  // parameter parsing
  while(1)
  {
    int option_index = 0, c = 0;
    static struct option long_options[] = {
        {"h", no_argument, 0, 0},
        {"help", no_argument, 0, 0},
        {"d", required_argument, 0, 0},
        {"device", required_argument, 0, 0},
        {0, 0, 0, 0}
    };

    // parsing all parameters according to the list above is sufficent
    c = getopt_long_only(argc, argv, "", long_options, &option_index);

    // no more options to parse
    if (c == -1) break;

    // unrecognized option
    if (c == '?') {
      Usage(argv[0]);
      return 0;
    }

    // dispatch the given options
    switch(option_index) {
    // h, help
    case 0:
    case 1:
      Usage(argv[0]);
      return 0;
      break;

    // d, device
    case 2:
    case 3:
      if (strlen(optarg) == 1)
      {
        char tmp[20];
        sprintf(tmp, "/dev/ttyUSB%s", optarg);
        dev_name = strdup(tmp);
      }
      else
        dev_name = strdup(optarg);
      break;

    default:
      Usage(argv[0]);
      return 0;
    }
  }
#endif

  // Initialize PortHandler instance
  // Set the port path
  // Get methods and members of PortHandlerLinux or PortHandlerWindows
  dynamixel::PortHandler *portHandler = dynamixel::PortHandler::getPortHandler(dev_name);

  // Open port
  if (portHandler->openPort())
  {
    printf("Succeeded to open the port!\n\n");
    printf(" - Device Name : %s\n", dev_name);
    printf(" - Baudrate    : %d\n\n", portHandler->getBaudRate());
  }
  else
  {
    printf("Failed to open the port! [%s]\n", dev_name);
    printf("Press any key to terminate...\n");
    getch();
    return 0;
  }

  char    input[128];
  char    cmd[80];
  char    param[20][30];
  int     num_param;
  char    *token;
  uint8_t dxl_error;

  while(1)
  {
    printf("[CMD] ");
    fgets(input, sizeof(input), stdin);
    char *p;
    if ((p = strchr(input, '\n'))!= NULL) *p = '\0';
    fflush(stdin);

    if (strlen(input) == 0) continue;

    token = strtok(input, " ");

    if (token == 0) continue;

    strcpy(cmd, token);
    token = strtok(0, " ");
    num_param = 0;
    while(token != 0)
    {
      strcpy(param[num_param++], token);
      token = strtok(0, " ");
    }

    if (strcmp(cmd, "help") == 0 || strcmp(cmd, "h") == 0 || strcmp(cmd, "?") == 0)
    {
      Help();
    }
    else if (strcmp(cmd, "baud") == 0)
    {
      if (num_param == 1)
      {
        if (portHandler->setBaudRate(atoi(param[0])) == false)
          fprintf(stderr, " Failed to change baudrate! \n");
        else
          fprintf(stderr, " Success to change baudrate! [ BAUD RATE: %d ]\n", atoi(param[0]));
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
        continue;
      }
    }
    else if (strcmp(cmd, "exit") == 0)
    {
      portHandler->closePort();
      return 0;
    }
    else if (strcmp(cmd, "scan") == 0)
    {
      Scan(portHandler, packetHandler1, packetHandler2);
    }
    else if (strcmp(cmd, "ping") == 0)
    {
      uint16_t dxl_model_num;

      if (num_param == 0)
      {
        fprintf(stderr, " Invalid parameters! \n");
        continue;
      }

      fprintf(stderr, "\n");
      fprintf(stderr, "ping Using Protocol 1.0\n");
      for (int i = 0; i < num_param; i++)
      {
        if (packetHandler1->ping(portHandler, atoi(param[i]), &dxl_model_num, &dxl_error) == COMM_SUCCESS)
        {
          fprintf(stderr, "\n                                          ... SUCCESS \r");
          fprintf(stderr, " [ID:%.3d] Model No : %.5d \n", atoi(param[i]), dxl_model_num);
        }
        else
        {
          fprintf(stderr, "\n                                          ... FAIL \r");
          fprintf(stderr, " [ID:%.3d] \n", atoi(param[i]));
        }
      }
      fprintf(stderr, "\n");

      fprintf(stderr, "\n");
      fprintf(stderr, "ping Using Protocol 2.0\n");
      for (int i = 0; i < num_param; i++)
      {
        if (packetHandler2->ping(portHandler, atoi(param[i]), &dxl_model_num, &dxl_error) == COMM_SUCCESS)
        {
          fprintf(stderr, "\n                                          ... SUCCESS \r");
          fprintf(stderr, " [ID:%.3d] Model No : %.5d \n", atoi(param[i]), dxl_model_num);
        }
        else
        {
          fprintf(stderr, "\n                                          ... FAIL \r");
          fprintf(stderr, " [ID:%.3d] \n", atoi(param[i]));
        }
      }
      fprintf(stderr, "\n");
    }
    else if (strcmp(cmd, "bp") == 0)
    {
      if (num_param == 0)
      {
        std::vector<unsigned char> vec;

        int dxl_comm_result = packetHandler2->broadcastPing(portHandler, vec);
        if (dxl_comm_result != COMM_SUCCESS) packetHandler2->printTxRxResult(dxl_comm_result);

        for (unsigned int i = 0; i < vec.size(); i++)
        {
          fprintf(stderr, "\n                                          ... SUCCESS \r");
          fprintf(stderr, " [ID:%.3d] \n", vec.at(i));
        }
        printf("\n");
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "wrb1") == 0 || strcmp(cmd, "w1") == 0)
    {
      if (num_param == 3)
      {
        Write(portHandler, packetHandler1, atoi(param[0]), atoi(param[1]), 1, atoi(param[2]));
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "wrb2") == 0 || strcmp(cmd, "w2") == 0)
    {
      if (num_param == 3)
      {
        Write(portHandler, packetHandler2, atoi(param[0]), atoi(param[1]), 1, atoi(param[2]));
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "wrw1") == 0)
    {
      if (num_param == 3)
      {
        Write(portHandler, packetHandler1, atoi(param[0]), atoi(param[1]), 2, atoi(param[2]));
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "wrw2") == 0)
    {
      if (num_param == 3)
      {
        Write(portHandler, packetHandler2, atoi(param[0]), atoi(param[1]), 2, atoi(param[2]));
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "wrd2") == 0)
    {
      if (num_param == 3)
      {
        Write(portHandler, packetHandler2, atoi(param[0]), atoi(param[1]), 4, atoi(param[2]));
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "rdb1") == 0)
    {
      if (num_param == 2)
      {
        Read(portHandler, packetHandler1, atoi(param[0]), atoi(param[1]), 1);
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "rdb2") == 0)
    {
      if (num_param == 2)
      {
        Read(portHandler, packetHandler2, atoi(param[0]), atoi(param[1]), 1);
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "rdw1") == 0)
    {
      if (num_param == 2)
      {
        Read(portHandler, packetHandler1, atoi(param[0]), atoi(param[1]), 2);
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "rdw2") == 0)
    {
      if (num_param == 2)
      {
        Read(portHandler, packetHandler2, atoi(param[0]), atoi(param[1]), 2);
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "rdd2") == 0)
    {
      if (num_param == 2)
      {
        Read(portHandler, packetHandler2, atoi(param[0]), atoi(param[1]), 4);
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "r1") == 0)
    {
      if (num_param == 3)
      {
        Dump(portHandler, packetHandler1, atoi(param[0]), atoi(param[1]), atoi(param[2]));
      }
      else{
        fprintf(stderr, " Invalid parameters! \n");}
    }
    else if (strcmp(cmd, "r2") == 0)
    {
      if (num_param == 3)
      {
        Dump(portHandler, packetHandler2, atoi(param[0]), atoi(param[1]), atoi(param[2]));
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "reboot2") == 0 || strcmp(cmd, "rbt2") == 0)
    {
      if (num_param == 1)
      {
        int dxl_comm_result = packetHandler2->reboot(portHandler, atoi(param[0]), &dxl_error);
        if (dxl_comm_result == COMM_SUCCESS)
        {
          if (dxl_error != 0) packetHandler2->printRxPacketError(dxl_error);
          fprintf(stderr, "\n Success to reboot! \n\n");
        }
        else
        {
          packetHandler2->printTxRxResult(dxl_comm_result);
          fprintf(stderr, "\n Fail to reboot! \n\n");
        }
      }
      else
      {
          fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "reset1") == 0 || strcmp(cmd, "rst1") == 0)
    {
      if (num_param == 1)
      {
        int dxl_comm_result = packetHandler1->factoryReset(portHandler, atoi(param[0]), 0x00, &dxl_error);
        if (dxl_comm_result == COMM_SUCCESS)
        {
          if (dxl_error != 0)
            packetHandler1->printRxPacketError(dxl_error);
          fprintf(stderr, "\n Success to reset! \n\n");
        }
        else
        {
          packetHandler1->printTxRxResult(dxl_comm_result);
          fprintf(stderr, "\n Fail to reset! \n\n");
        }
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else if (strcmp(cmd, "reset2") == 0 || strcmp(cmd, "rst2") == 0)
    {
      if (num_param == 2)
      {
        int dxl_comm_result = packetHandler2->factoryReset(portHandler, atoi(param[0]), atoi(param[1]), &dxl_error);
        if (dxl_comm_result == COMM_SUCCESS)
        {
          if (dxl_error != 0) packetHandler2->printRxPacketError(dxl_error);
          fprintf(stderr, "\n Success to reset! \n\n");
        }
        else
        {
          packetHandler2->printTxRxResult(dxl_comm_result);
          fprintf(stderr, "\n Fail to reset! \n\n");
        }
      }
      else
      {
        fprintf(stderr, " Invalid parameters! \n");
      }
    }
    else
    {
      printf(" Bad command! Please input 'help'.\n");
    }
  }
}