Edit on GitHub
    
    
    
    
    
Python Windows
Recommended Editor
Compiler and Builder

- 
    Download Python3 for Windows, and be sure to install it to your path when prompted.  
Building the Library
- 
    Navigate to the [ DynamixelSDK python folder] in the Windows command prompt. (cd [DynamixelSDK folder]\python). Then, run the installation by entering the following command on the command prompt from inside the folder (pip install .).  
Building and Running the Sample Code
The DYNAMIXEL SDK example code for Python uses the library files installed in the previous step.
Run Example
- 
    Open the pythonfolder using your preffered development environment and modify any settings that may be needed for accurate control of the DYNAMIXEL servos you’ll be using. 
- 
    Run the read_write.pyexample to check your installation. 
- 
    Or run the script manually through the command prompt.